sl_bt_evt_connection_phy_statusConnection#

Indicates that PHY update procedure is completed.

Data Structures

struct  

sl_bt_evt_connection_phy_status_s

Data structure of the phy_status event.

Macros

#define  

sl_bt_evt_connection_phy_status_id   0x040600a0

Identifier of the phy_status event.

Detailed Description#

Indicates that PHY update procedure is completed.


Data Structure Documentation#

◆sl_bt_evt_connection_phy_status_s#

struct sl_bt_evt_connection_phy_status_s

Data structure of the phy_status event.

Data Fields

name

description

uint8_t

connection

Connection handle

uint8_t

phy

Current active PHY. See values from sl_bt_connection_set_preferred_phy command.