Connection#

Connection.

Modules

Transmit Power Reporting Constants

sl_bt_evt_connection_opened

Indicates that a new connection was opened.

sl_bt_evt_connection_parameters

Triggered whenever the connection parameters are changed and at any time a connection is established.

sl_bt_evt_connection_phy_status

Indicates that PHY update procedure is completed.

sl_bt_evt_connection_rssi

Triggered when an connection_get_rssi command has completed.

sl_bt_evt_connection_get_remote_tx_power_completed

Indicates that reading remote transmit power initiated by sl_bt_connection_get_remote_tx_power command has completed.

sl_bt_evt_connection_tx_power

Reports a transmit power change on the local device of a connection if transmit power reporting has been enabled.

sl_bt_evt_connection_remote_tx_power

Reports a transmit power change on the remote device of a connection if transmit power reporting has been enabled.

sl_bt_evt_connection_closed

Indicates that a connection was either closed or that no connection was established from a high duty cycle directed advertising.

sl_bt_evt_connection_remote_used_features

List of link layer features supported by the remote device.

Enumerations

enum  

sl_bt_connection_security_t { sl_bt_connection_mode1_level1 = 0x0, sl_bt_connection_mode1_level2 = 0x1, sl_bt_connection_mode1_level3 = 0x2, sl_bt_connection_mode1_level4 = 0x3 }

Indicate the Bluetooth Security Mode.

enum  

sl_bt_connection_power_reporting_mode_t { sl_bt_connection_power_reporting_disable = 0x0, sl_bt_connection_power_reporting_enable = 0x1 }

These values define transmit power reporting modes in LE power control.

enum  

sl_bt_connection_tx_power_flag_t { sl_bt_connection_tx_power_flag_none = 0x0, sl_bt_connection_tx_power_at_minimum = 0x1, sl_bt_connection_tx_power_at_maximum = 0x2 }

This enum defines the flag values for a reported transmit power level.

Functions

sl_status_t 

sl_bt_connection_set_default_parameters (uint16_t min_interval, uint16_t max_interval, uint16_t latency, uint16_t timeout, uint16_t min_ce_length, uint16_t max_ce_length)

sl_status_t 

sl_bt_connection_set_default_preferred_phy (uint8_t preferred_phy, uint8_t accepted_phy)

sl_status_t 

sl_bt_connection_open (bd_addr address, uint8_t address_type, uint8_t initiating_phy, uint8_t *connection)

sl_status_t 

sl_bt_connection_set_parameters (uint8_t connection, uint16_t min_interval, uint16_t max_interval, uint16_t latency, uint16_t timeout, uint16_t min_ce_length, uint16_t max_ce_length)

sl_status_t 

sl_bt_connection_set_preferred_phy (uint8_t connection, uint8_t preferred_phy, uint8_t accepted_phy)

sl_status_t 

sl_bt_connection_disable_slave_latency (uint8_t connection, uint8_t disable)

sl_status_t 

sl_bt_connection_get_rssi (uint8_t connection)

sl_status_t 

sl_bt_connection_read_channel_map (uint8_t connection, size_t max_channel_map_size, size_t *channel_map_len, uint8_t *channel_map)

sl_status_t 

sl_bt_connection_set_power_reporting (uint8_t connection, uint8_t mode)

sl_status_t 

sl_bt_connection_set_remote_power_reporting (uint8_t connection, uint8_t mode)

sl_status_t 

sl_bt_connection_get_tx_power (uint8_t connection, uint8_t phy, int8_t *current_level, int8_t *max_level)

sl_status_t 

sl_bt_connection_get_remote_tx_power (uint8_t connection, uint8_t phy)

sl_status_t 

sl_bt_connection_close (uint8_t connection)

sl_status_t 

sl_bt_connection_read_remote_used_features (uint8_t connection)

sl_status_t 

sl_bt_connection_get_security_status (uint8_t connection, uint8_t *security_mode, uint8_t *key_size, uint8_t *bonding_handle)

Detailed Description#

Connection.

The commands and events in this class are related to managing connection establishment, parameter setting, and disconnection procedures.

Enumeration Type Documentation#

◆sl_bt_connection_security_t#

enum sl_bt_connection_security_t

Indicate the Bluetooth Security Mode.

Enumerator

sl_bt_connection_mode1_level1 

(0x0) No security

sl_bt_connection_mode1_level2 

(0x1) Unauthenticated pairing with encryption

sl_bt_connection_mode1_level3 

(0x2) Authenticated pairing with encryption

sl_bt_connection_mode1_level4 

(0x3) Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key

◆sl_bt_connection_power_reporting_mode_t#

enum sl_bt_connection_power_reporting_mode_t

These values define transmit power reporting modes in LE power control.

Enumerator

sl_bt_connection_power_reporting_disable 

(0x0) Disable transmit power reporting

sl_bt_connection_power_reporting_enable 

(0x1) Enable transmit power reporting

◆sl_bt_connection_tx_power_flag_t#

enum sl_bt_connection_tx_power_flag_t

This enum defines the flag values for a reported transmit power level.

Enumerator

sl_bt_connection_tx_power_flag_none 

(0x0) No flag is defined for the reported TX power level

sl_bt_connection_tx_power_at_minimum 

(0x1) Transmit power level is at minimum level.

sl_bt_connection_tx_power_at_maximum 

(0x2) Transmit power level is at maximum level.

Function Documentation#

◆sl_bt_connection_set_default_parameters()#

sl_status_t sl_bt_connection_set_default_parameters

(

uint16_t 

min_interval,

uint16_t 

max_interval,

uint16_t 

latency,

uint16_t 

timeout,

uint16_t 

min_ce_length,

uint16_t 

max_ce_length

)

Set default Bluetooth connection parameters. The values are valid for all subsequent connections initiated by this device.

min_ce_length and max_ce_length specify the preference of the connection event length so that the Link Layer can prioritize tasks accordingly in simultaneous connections, or scanning and so on. A connection event starts at an anchor point of a connection interval and lasts until the lesser of max_ce_length and the actual connection interval. Packets that do not fit into the connection event will be sent in the next connection interval.

To change parameters of an already established connection, use the command sl_bt_connection_set_parameters.

Parameters

[in]

min_interval

Minimum value for the connection event interval. This must be set less than or equal to max_interval.

  • Time = Value x 1.25 ms

  • Range: 0x0006 to 0x0c80

  • Time Range: 7.5 ms to 4 s

  • Default value: 20 ms

[in]

max_interval

Maximum value for the connection event interval. This must be set greater than or equal to min_interval.

  • Time = Value x 1.25 ms

  • Range: 0x0006 to 0x0c80

  • Time Range: 7.5 ms to 4 s

  • Default value: 50 ms

[in]

latency

Peripheral latency, which defines how many connection intervals the peripheral can skip if it has no data to send

  • Range: 0x0000 to 0x01f3

  • Default value: 0

[in]

timeout

Supervision timeout, which defines the time that the connection is maintained although the devices can't communicate at the currently configured connection intervals.

  • Range: 0x000a to 0x0c80

  • Time = Value x 10 ms

  • Time Range: 100 ms to 32 s

  • The value in milliseconds must be larger than (1 + Set the supervision timeout at a value which allows communication attempts over at least a few connection intervals.

Default value: 1000 ms

[in]

min_ce_length

Minimum length of the connection event. It must be less than or equal to max_ce_length. This value defines the minimum time that should be given to the connection event in a situation where other tasks need to run immediately after the connection event. When the value is very small, the connection event still has at least one TX/RX operation. If this value is increased, more time is reserved for the connection event so it can transmit and receive more packets in a connection interval. Use the default value if the application doesn't care about the connection event length or doesn't want to do fine tuning.

  • Time = Value x 0.625 ms

  • Range: 0x0000 to 0xffff

  • Default value: 0x0000

[in]

max_ce_length

Maximum length of the connection event. It must be greater than or equal to min_ce_length. This value is used for limiting the connection event length so that a connection that has large amounts of data to transmit or receive doesn't block other tasks. Limiting the connection event is a hard stop. If there is no enough time to send or receive a packet, the connection event will be closed. If the value is set to 0, the connection event still has at least one TX/RX operation. This is useful to limit power consumption or leave more time to other tasks. Use the default value if the application doesn't care about the connection event length or doesn't want to do fine tuning.

  • Time = Value x 0.625 ms

  • Range: 0x0000 to 0xffff

  • Default value: 0xffff

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_connection_set_default_preferred_phy()#

sl_status_t sl_bt_connection_set_default_preferred_phy

(

uint8_t 

preferred_phy,

uint8_t 

accepted_phy

)

Set default preferred and accepted PHYs. PHY settings will be used for all subsequent connections. Non-preferred PHY can also be set if the remote device does not accept any of the preferred PHYs.

The parameter accepted_phy is used to specify PHYs that the stack can accept in a remotely-initiated PHY update request. A PHY update will not happen if none of the accepted PHYs are present in the request.

NOTE: 2M and Coded PHYs are not supported by all devices.

Parameters

[in]

preferred_phy

Preferred PHYs. This parameter is a bitfield and multiple PHYs can be set.

  • 0x01: 1M PHY

  • 0x02: 2M PHY

  • 0x04: Coded PHY

  • 0xff: Any PHYs

  • Default: 0xff (no preference)

[in]

accepted_phy

Accepted PHYs in remotely-initiated PHY update request. This parameter is a bitfield and multiple PHYs can be set.

  • 0x01: 1M PHY

  • 0x02: 2M PHY

  • 0x04: Coded PHY

  • 0xff: Any PHYs

  • Default: 0xff (all PHYs accepted)

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_connection_open()#

sl_status_t sl_bt_connection_open

(

bd_addr

address,

uint8_t 

address_type,

uint8_t 

initiating_phy,

uint8_t * 

connection

)

Connect to an advertising device with the specified initiating PHY on which connectable advertisements on primary advertising channels are received. The Bluetooth stack will enter a state where it continuously scans for the connectable advertising packets from the remote device, which matches the Bluetooth address given as a parameter. Scan parameters set in sl_bt_scanner_set_timing are used in this operation. Upon receiving the advertising packet, the module will send a connection request packet to the target device to initiate a Bluetooth connection. To cancel an ongoing connection process, use sl_bt_connection_close command with the handle received in response from this command.

A connection is opened in no-security mode. If the GATT client needs to read or write the attributes on GATT server requiring encryption or authentication, it must first encrypt the connection using an appropriate authentication method.

If a connection can't be established, for example, the remote device has gone out of range, has entered into deep sleep, or is not advertising, the stack will try to connect forever. In this case, the application will not get an event related to the connection request. To recover from this situation, the application can implement a timeout and call sl_bt_connection_close to cancel the connection request.

This command fails with the connection limit exceeded error if the number of connections attempted exceeds the configured MAX_CONNECTIONS value.

This command fails with the invalid parameter error if the initiating PHY value is invalid or the device does not support PHY.

Subsequent calls of this command have to wait for the ongoing command to complete. A received event sl_bt_evt_connection_opened indicates that the connection opened successfully and a received event sl_bt_evt_connection_closed indicates that connection failures have occurred.

Parameters

[in]

address

Address of the device to connect to

[in]

address_type

Address type of the device to connect to. Values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address

  • sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address

[in]

initiating_phy

The initiating PHY. Values:

  • sl_bt_gap_phy_1m (0x1): 1M PHY

  • sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2)

[out]

connection

Handle that will be assigned to the connection after the connection is established. This handle is valid only if the result code of this response is 0 (zero).

ReturnsSL_STATUS_OK if successful. Error code otherwise. Events

  • sl_bt_evt_connection_opened - This event is triggered after the connection is opened and indicates whether the devices are already bonded and the role of the device in this connection.

  • sl_bt_evt_connection_parameters - This event indicates the connection parameters and security mode of the connection.

◆sl_bt_connection_set_parameters()#

sl_status_t sl_bt_connection_set_parameters

(

uint8_t 

connection,

uint16_t 

min_interval,

uint16_t 

max_interval,

uint16_t 

latency,

uint16_t 

timeout,

uint16_t 

min_ce_length,

uint16_t 

max_ce_length

)

Request a change in the connection parameters of a Bluetooth connection.

min_ce_length and max_ce_length specify the preference of the connection event length so that the Link Layer can prioritize tasks accordingly in simultaneous connections, or scanning and so on. A connection event starts at an anchor point of a connection interval and lasts until the lesser of max_ce_length and the actual connection interval. Packets that do not fit into the connection event will be sent in the next connection interval.

Parameters

[in]

connection

Connection Handle

[in]

min_interval

Minimum value for the connection event interval. This must be set less than or equal to max_interval.

  • Time = Value x 1.25 ms

  • Range: 0x0006 to 0x0c80

  • Time Range: 7.5 ms to 4 s

[in]

max_interval

Maximum value for the connection event interval. This must be set greater than or equal to min_interval.

  • Time = Value x 1.25 ms

  • Range: 0x0006 to 0x0c80

  • Time Range: 7.5 ms to 4 s

[in]

latency

Peripheral latency, which defines how many connection intervals the peripheral can skip if it has no data to send

  • Range: 0x0000 to 0x01f3

[in]

timeout

Supervision timeout, which defines the time that the connection is maintained although the devices can't communicate at the currently configured connection intervals.

  • Range: 0x000a to 0x0c80

  • Time = Value x 10 ms

  • Time Range: 100 ms to 32 s

  • The value in milliseconds must be larger than (1 + Set the supervision timeout at a value which allows communication attempts over at least a few connection intervals.

[in]

min_ce_length

Minimum length of the connection event. It must be less than or equal to max_ce_length. This value defines the minimum time that should be given to the connection event in a situation where other tasks need to run immediately after the connection event. When the value is very small, the connection event still has at least one TX/RX operation. If this value is increased, more time is reserved for the connection event so it can transmit and receive more packets in a connection interval. Use the default value if the application doesn't care about the connection event length or doesn't want to do fine tuning.

  • Time = Value x 0.625 ms

  • Range: 0x0000 to 0xffff

  • Default value: 0x0000

[in]

max_ce_length

Maximum length of the connection event. It must be greater than or equal to min_ce_length. This value is used for limiting the connection event length so that a connection that has large amounts of data to transmit or receive doesn't block other tasks. Limiting the connection event is a hard stop. If there is no enough time to send or receive a packet, the connection event will be closed. If the value is set to 0, the connection event still has at least one TX/RX operation. This is useful to limit power consumption or leave more time to other tasks. Use the default value if the application doesn't care about the connection event length or doesn't want to do fine tuning.

  • Time = Value x 0.625 ms

  • Range: 0x0000 to 0xffff

  • Default value: 0xffff

ReturnsSL_STATUS_OK if successful. Error code otherwise. Events

◆sl_bt_connection_set_preferred_phy()#

sl_status_t sl_bt_connection_set_preferred_phy

(

uint8_t 

connection,

uint8_t 

preferred_phy,

uint8_t 

accepted_phy

)

Set preferred and accepted PHYs for a given connection. Event sl_bt_evt_connection_phy_status is received when PHY update procedure is completed. Non-preferred PHY can also be set if remote device does not accept any of the preferred PHYs.

The parameter accepted_phy is used for specifying the PHYs that the stack can accept in a remote initiated PHY update request. A PHY update will not occur if none of the accepted PHYs presents in the request.

NOTE: 2M and Coded PHYs are not supported by all devices.

Parameters

[in]

connection

Connection handle

[in]

preferred_phy

Preferred PHYs. This parameter is a bitfield and multiple PHYs can be set.

  • 0x01: 1M PHY

  • 0x02: 2M PHY

  • 0x04: 125k Coded PHY (S=8)

  • 0x08: 500k Coded PHY (S=2)

  • Default: 0xff (no preference)

[in]

accepted_phy

Accepted PHYs in remotely-initiated PHY update requests. This parameter is a bitfield and multiple PHYs can be set.

  • 0x01: 1M PHY

  • 0x02: 2M PHY

  • 0x04: Coded PHY

  • 0xff: Any PHYs

  • Default: 0xff (all PHYs accepted)

ReturnsSL_STATUS_OK if successful. Error code otherwise. Events

◆sl_bt_connection_disable_slave_latency()#

sl_status_t sl_bt_connection_disable_slave_latency

(

uint8_t 

connection,

uint8_t 

disable

)

Temporarily enable or disable peripheral latency. Used only when Bluetooth device is acting as a peripheral. When peripheral latency is disabled, the peripheral latency connection parameter is not set to 0 but the device will wake up on every connection interval to receive and send packets.

Parameters

[in]

connection

Connection Handle

[in]

disable

0 enable, 1 disable peripheral latency. Default: 0

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_connection_get_rssi()#

sl_status_t sl_bt_connection_get_rssi

(

uint8_t 

connection

)

Get the latest RSSI value of a Bluetooth connection. The RSSI value will be reported in a sl_bt_evt_connection_rssi event.

Parameters

[in]

connection

Connection handle

ReturnsSL_STATUS_OK if successful. Error code otherwise. Events

◆sl_bt_connection_read_channel_map()#

sl_status_t sl_bt_connection_read_channel_map

(

uint8_t 

connection,

size_t 

max_channel_map_size,

size_t * 

channel_map_len,

uint8_t * 

channel_map

)

Read channel map for a specified connection.

Parameters

[in]

connection

Connection Handle

[in]

max_channel_map_size

Size of output buffer passed in channel_map

[out]

channel_map_len

On return, set to the length of output data written to channel_map

[out]

channel_map

This parameter is 5 bytes and contains 37 1-bit fields. The nth field (in the range 0 to 36) contains the value for the link layer channel index n.

  • 0: Channel n is unused

  • 1: Channel n is used

  • The most significant bits are reserved for future use.

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_connection_set_power_reporting()#

sl_status_t sl_bt_connection_set_power_reporting

(

uint8_t 

connection,

uint8_t 

mode

)

Enable or disable the transmit power reporting for the local device on a connection. When transmit power reporting is enabled, event sl_bt_evt_connection_tx_power is generated when transmit power on the local device changes.

By default, power reporting for local device is enabled.

Parameters

[in]

connection

Handle of the connection

[in]

mode

Transmit power reporting mode. Values:

  • sl_bt_connection_power_reporting_disable (0x0): Disable transmit power reporting

  • sl_bt_connection_power_reporting_enable (0x1): Enable transmit power reporting

ReturnsSL_STATUS_OK if successful. Error code otherwise. Events

◆sl_bt_connection_set_remote_power_reporting()#

sl_status_t sl_bt_connection_set_remote_power_reporting

(

uint8_t 

connection,

uint8_t 

mode

)

Enable or disable the transmit power reporting for the remote device on a connection. When transmit power reporting is enabled, event sl_bt_evt_connection_remote_tx_power is generated when transmit power on the remote device changes.

By default, power reporting for the remote device is disabled.

Parameters

[in]

connection

Handle of the connection

[in]

mode

Transmit power reporting mode. Values:

  • sl_bt_connection_power_reporting_disable (0x0): Disable transmit power reporting

  • sl_bt_connection_power_reporting_enable (0x1): Enable transmit power reporting

ReturnsSL_STATUS_OK if successful. Error code otherwise. Events

◆sl_bt_connection_get_tx_power()#

sl_status_t sl_bt_connection_get_tx_power

(

uint8_t 

connection,

uint8_t 

phy,

int8_t * 

current_level,

int8_t * 

max_level

)

Get the transmit power of the local device on the given connection and PHY.

Parameters

[in]

connection

Handle of the connection

[in]

phy

The PHY. Values:

  • sl_bt_gap_phy_coding_1m_uncoded (0x1): 1M PHY

  • sl_bt_gap_phy_coding_2m_uncoded (0x2): 2M PHY

  • sl_bt_gap_phy_coding_125k_coded (0x4): 125k Coded PHY (S=8)

  • sl_bt_gap_phy_coding_500k_coded (0x8): 500k Coded PHY (S=2)

[out]

current_level

The current transmit power level of the PHY on the connection. Values:

  • Range -127 to 20: The transmit power level in dBm

[out]

max_level

The maximum transmit power level of the PHY on the connection. Values: Range -127 to +20 in dBm.

ReturnsSL_STATUS_OK if successful. Error code otherwise.

◆sl_bt_connection_get_remote_tx_power()#

sl_status_t sl_bt_connection_get_remote_tx_power

(

uint8_t 

connection,

uint8_t 

phy

)

Get the transmit power of the remote device on the given connection and PHY. Transmit power levels are returned in event sl_bt_evt_connection_get_remote_tx_power_completed after the operation completed.

Parameters

[in]

connection

Handle of the connection

[in]

phy

The PHY. Values:

  • sl_bt_gap_phy_coding_1m_uncoded (0x1): 1M PHY

  • sl_bt_gap_phy_coding_2m_uncoded (0x2): 2M PHY

  • sl_bt_gap_phy_coding_125k_coded (0x4): 125k Coded PHY (S=8)

  • sl_bt_gap_phy_coding_500k_coded (0x8): 500k Coded PHY (S=2)

ReturnsSL_STATUS_OK if the command is accepted. Error code otherwise. Events

◆sl_bt_connection_close()#

sl_status_t sl_bt_connection_close

(

uint8_t 

connection

)

Close a Bluetooth connection or cancel an ongoing connection establishment process. The parameter is a connection handle which is reported in sl_bt_evt_connection_opened event or sl_bt_connection_open command response.

Parameters

[in]

connection

Handle of the connection to be closed

ReturnsSL_STATUS_OK if successful. Error code otherwise. Events

◆sl_bt_connection_read_remote_used_features()#

sl_status_t sl_bt_connection_read_remote_used_features

(

uint8_t 

connection

)

Read link layer features supported by the remote device.

Parameters

[in]

connection

Connection Handle

ReturnsSL_STATUS_OK if successful. Error code otherwise. Events

◆sl_bt_connection_get_security_status()#

sl_status_t sl_bt_connection_get_security_status

(

uint8_t 

connection,

uint8_t * 

security_mode,

uint8_t * 

key_size,

uint8_t * 

bonding_handle

)

Get the security status of the connection.

Parameters

[in]

connection

Connection handle

[out]

security_mode

Connection security mode. Values:

  • sl_bt_connection_mode1_level1 (0x0): No security

  • sl_bt_connection_mode1_level2 (0x1): Unauthenticated pairing with encryption

  • sl_bt_connection_mode1_level3 (0x2): Authenticated pairing with encryption

  • sl_bt_connection_mode1_level4 (0x3): Authenticated Secure Connections pairing with encryption using a 128-bit strength encryption key

[out]

key_size

The size of encryption key

[out]

bonding_handle

Bonding handle. Values:

  • SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding

  • Other: Bonding handle

ReturnsSL_STATUS_OK if successful. Error code otherwise.