GAP#

GAP.

Enumerations#

enum  

sl_bt_gap_address_type_t { sl_bt_gap_public_address = 0x0, sl_bt_gap_static_address = 0x1, sl_bt_gap_random_resolvable_address = 0x2, sl_bt_gap_random_nonresolvable_address = 0x3 }

 

These values define Bluetooth device address types.

 

enum  

sl_bt_gap_phy_t { sl_bt_gap_phy_1m = 0x1, sl_bt_gap_phy_2m = 0x2, sl_bt_gap_phy_coded = 0x4, sl_bt_gap_phy_any = 0xff }

 

Types of PHYs.

 

enum  

sl_bt_gap_phy_coding_t { sl_bt_gap_phy_coding_1m_uncoded = 0x1, sl_bt_gap_phy_coding_2m_uncoded = 0x2, sl_bt_gap_phy_coding_125k_coded = 0x4, sl_bt_gap_phy_coding_500k_coded = 0x8 }

 

PHY types with coding schemes.

 

Functions#

sl_status_t 

sl_bt_gap_set_privacy_mode (uint8_t privacy, uint8_t interval)

 

sl_status_t 

sl_bt_gap_set_data_channel_classification (size_t channel_map_len, const uint8_t *channel_map)

 

sl_status_t 

sl_bt_gap_enable_whitelisting (uint8_t enable)

 

Detailed Description#

GAP.

The commands and events in this class are related to the Generic Access Profile (GAP) in Bluetooth.

Enumeration Type Documentation#

◆ sl_bt_gap_address_type_t#

enum sl_bt_gap_address_type_t

These values define Bluetooth device address types.

Enumerator

sl_bt_gap_public_address 

(0x0) Public device address

sl_bt_gap_static_address 

(0x1) Static device address

sl_bt_gap_random_resolvable_address 

(0x2) Resolvable private random address

sl_bt_gap_random_nonresolvable_address 

(0x3) Non-resolvable private random address

◆ sl_bt_gap_phy_t#

enum sl_bt_gap_phy_t

Types of PHYs.

Enumerator

sl_bt_gap_phy_1m 

(0x1) 1M PHY

sl_bt_gap_phy_2m 

(0x2) 2M PHY

sl_bt_gap_phy_coded 

(0x4) Coded PHY, 125k (S=8) or 500k (S=2)

sl_bt_gap_phy_any 

(0xff) Any PHYs the device supports

◆ sl_bt_gap_phy_coding_t#

enum sl_bt_gap_phy_coding_t

PHY types with coding schemes.

Enumerator

sl_bt_gap_phy_coding_1m_uncoded 

(0x1) 1M PHY

sl_bt_gap_phy_coding_2m_uncoded 

(0x2) 2M PHY

sl_bt_gap_phy_coding_125k_coded 

(0x4) 125k Coded PHY (S=8)

sl_bt_gap_phy_coding_500k_coded 

(0x8) 500k Coded PHY (S=2)

Function Documentation#

◆ sl_bt_gap_set_privacy_mode()#

sl_status_t sl_bt_gap_set_privacy_mode

(

uint8_t 

privacy,

uint8_t 

interval 

)

Enable or disable the privacy feature on all GAP roles. New privacy mode will take effect for advertising next time advertising is enabled, for scanning next time scanning is enabled, and for initiating on the next open connection command.

When privacy is enabled and the device is advertising or scanning, the stack will maintain a periodic timer with the specified time interval as a timeout value. At each timeout, the stack generates a new resolvable private address and uses it in scanning requests. For advertisers, the stack generates a new resolvable or non-resolvable private address and uses it in advertising data packets for each advertising set if its address is not application-managed, i.e., the address was not set by the application (with the sl_bt_advertiser_set_random_address command). The application is fully responsible for application-managed advertiser addresses. For an application-managed resolvable private address, the application should schedule periodic address updates for enhancing the privacy. It is recommended to use different schedules for different advertising sets.

Disabling the privacy during active advertising or scanning is not allowed.

By default, privacy feature is disabled.

Parameters

[in]

privacy

Values:

  • 0: Disable privacy

  • 1: Enable privacy

[in]

interval

The minimum time interval between a private address change. This parameter is ignored if this command is issued to disable privacy mode. Values:

  • 0: Use default interval, 15 minutes

  • others: The time interval in minutes

Returns

SL_STATUS_OK if successful. Error code otherwise.

◆ sl_bt_gap_set_data_channel_classification()#

sl_status_t sl_bt_gap_set_data_channel_classification

(

size_t 

channel_map_len,

const uint8_t * 

channel_map 

)

Specify a channel classification for data channels. This classification persists until overwritten with a subsequent command or until the system is reset.

Parameters

[in]

channel_map_len

Length of data in channel_map

[in]

channel_map

This parameter is 5 bytes and contains 37 1-bit fields.

The nth field (in the range 0 to 36) contains the value for the link layer channel index n.

  • 0: Channel n is bad.

  • 1: Channel n is unknown.

The rest of most significant bits are reserved for future use and must be set to 0.

At least two channels shall be marked as unknown.

Returns

SL_STATUS_OK if successful. Error code otherwise.

◆ sl_bt_gap_enable_whitelisting()#

sl_status_t sl_bt_gap_enable_whitelisting

(

uint8_t 

enable

)

Enable or disable accept list filtering. The setting will be effective the next time that scanning is enabled. To add devices to the accept list, either bond with the device or add it manually with sl_bt_sm_add_to_whitelist.

Parameters

[in]

enable

1 enable, 0 disable accept list filtering.

Returns

SL_STATUS_OK if successful. Error code otherwise.