GATT Descriptor Property FlagsGATT Database#

Macros

#define 

SL_BT_GATTDB_DESCRIPTOR_READ   0x1

#define 

SL_BT_GATTDB_DESCRIPTOR_WRITE   0x2

#define 

SL_BT_GATTDB_DESCRIPTOR_LOCAL_ONLY   0x200

Detailed Description#

This enum defines the property flags for GATT characteristic descriptors.

Macro Definition Documentation#

◆SL_BT_GATTDB_DESCRIPTOR_READ#

#define SL_BT_GATTDB_DESCRIPTOR_READ   0x1

A GATT client can read the descriptor value.

◆SL_BT_GATTDB_DESCRIPTOR_WRITE#

#define SL_BT_GATTDB_DESCRIPTOR_WRITE   0x2

A GATT client can write the descriptor value.

◆SL_BT_GATTDB_DESCRIPTOR_LOCAL_ONLY#

#define SL_BT_GATTDB_DESCRIPTOR_LOCAL_ONLY   0x200

The descriptor is local only and should be invisible to GATT clients.