sl_bt_evt_sync_closedSynchronization#

Indicates that periodic advertising synchronization was lost or a synchronization establishment procedure was canceled.

Data Structures

struct  

sl_bt_evt_sync_closed_s

Data structure of the closed event.

Macros

#define  

sl_bt_evt_sync_closed_id   0x014200a0

Identifier of the closed event.

Detailed Description#

Indicates that periodic advertising synchronization was lost or a synchronization establishment procedure was canceled.

The synchronization establishment procedure can be canceled explicitly by the application by issuing command sl_bt_sync_close, or internally due to synchronization failing. Synchronization can fail for example due to incompatible sync CTE type.


Data Structure Documentation#

◆sl_bt_evt_sync_closed_s#

struct sl_bt_evt_sync_closed_s

Data structure of the closed event.

Data Fields

uint16_t

reason

SL_STATUS_OK if successful. Error code otherwise.

uint16_t

sync

Periodic advertising synchronization handle