sl_bt_evt_sync_openedSynchronization#

Indicates that a periodic advertising synchronization has been opened.

Data Structures

struct  

sl_bt_evt_sync_opened_s

Data structure of the opened event.

Macros

#define  

sl_bt_evt_sync_opened_id   0x004200a0

Identifier of the opened event.

Detailed Description#

Indicates that a periodic advertising synchronization has been opened.


Data Structure Documentation#

◆sl_bt_evt_sync_opened_s#

struct sl_bt_evt_sync_opened_s

Data structure of the opened event.

Data Fields

name

description

uint16_t

sync

Periodic advertising synchronization handle

uint8_t

adv_sid

Advertising set identifier

bd_addr

address

Address of the advertiser

uint8_t

address_type

Advertiser address type. Values:

  • 0: Public address

  • 1: Random address

uint8_t

adv_phy

The advertiser PHY. Values:

  • sl_bt_gap_phy_1m (0x1): 1M PHY

  • sl_bt_gap_phy_2m (0x2): 2M PHY

  • sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2)

uint16_t

adv_interval

The periodic advertising interval. Value in units of 1.25 ms

  • Range: 0x06 to 0xFFFF

  • Time range: 7.5 ms to 81.92 s

uint16_t

clock_accuracy

Enum sl_bt_sync_advertiser_clock_accuracy_t. The advertiser clock accuracy.

uint8_t

bonding

Bonding handle. Values:

  • SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding

  • Other: Bonding handle