sl_bt_evt_system_bootSystem#

Indicates that the device has started and the radio is ready.

Data Structures

struct  

sl_bt_evt_system_boot_s

Data structure of the boot event.

Macros

#define 

sl_bt_evt_system_boot_id   0x000100a0

Identifier of the boot event.

Detailed Description#

Indicates that the device has started and the radio is ready.

This event carries the firmware build number and other software and hardware identification codes.


Data Structure Documentation#

◆sl_bt_evt_system_boot_s#

struct sl_bt_evt_system_boot_s

Data structure of the boot event.

Data Fields

uint16_t

major

Major release version

uint16_t

minor

Minor release version

uint16_t

patch

Patch release number

uint16_t

build

Build number

uint32_t

bootloader

Unused. Ignore this field.

uint16_t

hw

Hardware type: the major chip revision number in the most significant byte and the minor revision in the least significant byte

uint32_t

hash

Version hash