sl_bt_evt_system_external_signalSystem#

Indicates that the external signals have been received.

Data Structures

struct  

sl_bt_evt_system_external_signal_s

Data structure of the external_signal event.

Macros

#define 

sl_bt_evt_system_external_signal_id   0x030100a0

Identifier of the external_signal event.

Detailed Description#

Indicates that the external signals have been received.

External signals are generated from the native application.


Data Structure Documentation#

◆sl_bt_evt_system_external_signal_s#

struct sl_bt_evt_system_external_signal_s

Data structure of the external_signal event.

Data Fields

uint32_t

extsignals

Bitmask of external signals received since last event.