BGAPI Types#
Common types in BGAPI protocol.
Data Structures | |
struct | |
Variable-length uint8_t array. Maximum length: 255. | |
struct | |
Variable-length int8_t array. Maximum length: 65535. | |
struct | |
Bluetooth address. | |
struct | |
128-bit UUID | |
struct | |
128-bit AES key | |
struct | |
16-bit UUID | |
struct | |
64-bit UUID | |
Macros | ||
# define | ||
The length of a BGAPI message header which is 4 bytes. | ||
#define | SL_BGAPI_MSG_DEVICE_TYPE(HDR) ((HDR) & 0x38) | |
Get the device type of a BGAPI message. | ||
#define | SL_BGAPI_MSG_ID(HDR) ((HDR) & 0xffff00f8) | |
Get the identifier of a BGAPI message including device type, class ID, message type and message ID. | ||
#define | SL_BGAPI_MSG_LEN(HDR) ((((HDR) & 0x7) << 8) | (((HDR) & 0xff00) >> 8)) |
Get the data payload length in a BGAPI message. | ||
# define | SL_BGAPI_BIT_ENCRYPTED (1 << 6) | |
The bit indicating whether data of a BGAPI message is encrypted. | ||
#define | SL_BGAPI_MSG_ENCRYPTED(HDR) ((HDR)&SL_BGAPI_BIT_ENCRYPTED) | |
Check whether data of a BGAPI message is encrypted. | ||
Detailed Description#
Common types in BGAPI protocol.
Data Structure Documentation#
◆uint8array#
struct uint8array |
Variable-length uint8_t array. Maximum length: 255.
Data Fields | |
|---|---|
uint8_t | |
len | Number of bytes stored in |
uint8_t | |
data[] | Data bytes |
◆byte_array#
struct byte_array |
Variable-length int8_t array. Maximum length: 65535.
Data Fields | |
|---|---|
uint16_t | |
len | Number of bytes stored in |
int8_t | |
data[] | Data bytes |
◆bd_addr#
struct bd_addr |
Bluetooth address.
Data Fields |
|---|
uint8_t |
addr[6] |
Bluetooth address in reverse byte order. |
◆uuid_128#
struct uuid_128 |
128-bit UUID
Data Fields | |
|---|---|
uint8_t | |
data[16] | 128-bit UUID |
◆aes_key_128#
struct aes_key_128 |
128-bit AES key
Data Fields | |
|---|---|
uint8_t | |
data[16] | 128-bit AES key |
◆sl_bt_uuid_16_t#
struct sl_bt_uuid_16_t |
16-bit UUID
Data Fields | |
|---|---|
uint8_t | |
data[2] | 16-bit UUID |
◆sl_bt_uuid_64_t#
struct sl_bt_uuid_64_t |
64-bit UUID
Data Fields | |
|---|---|
uint8_t | |
data[8] | 64-bit UUID |
Macro Definition Documentation#
◆SL_BGAPI_MSG_DEVICE_TYPE#
#define SL_BGAPI_MSG_DEVICE_TYPE | ( |
| ) | ((HDR) & 0x38) |
Get the device type of a BGAPI message.
Parameters
| The header of the message as a uint32_t integer |
◆SL_BGAPI_MSG_ID#
#define SL_BGAPI_MSG_ID | ( |
| ) | ((HDR) & 0xffff00f8) |
Get the identifier of a BGAPI message including device type, class ID, message type and message ID.
Parameters
| The header of the message as a uint32_t integer |
◆SL_BGAPI_MSG_LEN#
#define SL_BGAPI_MSG_LEN | ( |
| ) | ((((HDR) & 0x7) << 8) | (((HDR) & 0xff00) >> 8)) |
Get the data payload length in a BGAPI message.
Parameters
| The header of the message as a uint32_t integer |
◆SL_BGAPI_MSG_ENCRYPTED#
#define SL_BGAPI_MSG_ENCRYPTED | ( |
| ) | ((HDR)&SL_BGAPI_BIT_ENCRYPTED) |
Check whether data of a BGAPI message is encrypted.
Parameters
| The BGAPI header of the message as a uint32_t integer |