Coexistence#
Coexistence.
Enumerations | |
enum | sl_bt_coex_option_t { sl_bt_coex_option_enable = 0x100, |
sl_bt_coex_option_tx_abort = 0x400, | |
sl_bt_coex_option_high_priority = 0x800 | |
} | |
Coexistence configuration options. | |
Functions | |
sl_status_t | sl_bt_coex_set_options (uint32_t mask, uint32_t options) |
sl_status_t | sl_bt_coex_set_parameters (uint8_t priority, uint8_t request, uint8_t pwm_period, uint8_t pwm_dutycycle) |
sl_status_t | sl_bt_coex_set_directional_priority_pulse (uint8_t pulse) |
sl_status_t | sl_bt_coex_get_parameters (uint8_t *priority, uint8_t *request, uint8_t *pwm_period, uint8_t *pwm_dutycycle) |
sl_status_t | sl_bt_coex_get_counters (uint8_t reset, size_t max_counters_size, size_t *counters_len, uint8_t *counters) |
Detailed Description#
Coexistence.
Coexistence BGAPI class. Coexistence interface is enabled and initialized with sl_bt_init_coex_hal function.
Enumeration Type Documentation#
◆sl_bt_coex_option_t#
enum sl_bt_coex_option_t |
Coexistence configuration options.
Enumerator | |
|---|---|
sl_bt_coex_option_enable | (0x100) Enable coexistence feature |
sl_bt_coex_option_tx_abort | (0x400) Abort transmission if grant is denied |
sl_bt_coex_option_high_priority | (0x800) Enable priority signal |
Function Documentation#
◆sl_bt_coex_set_options()#
sl_status_t sl_bt_coex_set_options | ( | uint32_t |
|
uint32_t |
| ||
) |
Configure coexistence options at runtime.
Parameters
[in] |
| Bitmask of following coexistence options to change* sl_bt_coex_option_enable : (0x100) Enable coexistence feature |
sl_bt_coex_option_tx_abort : (0x400) Abort transmission if grant is denied
sl_bt_coex_option_high_priority : (0x800) Enable priority signal | | [in] |
options| Bitmask of following coexistence option values to set* sl_bt_coex_option_enable : (0x100) Enable coexistence featuresl_bt_coex_option_tx_abort : (0x400) Abort transmission if grant is denied
sl_bt_coex_option_high_priority : (0x800) Enable priority signal |
ReturnsSL_STATUS_OK if successful. Error code otherwise.
◆sl_bt_coex_set_parameters()#
sl_status_t sl_bt_coex_set_parameters | ( | uint8_t |
|
uint8_t |
| ||
uint8_t |
| ||
uint8_t |
| ||
) |
Configure coexistence parameters.
Parameters
[in] |
| Coexistence priority threshold. Coexistence priority is toggled if priority is below this value. |
[in] |
| Coexistence request threshold. Coexistence request is toggled if priority is below this value. |
[in] |
| PWM functionality period length in 1 ms units |
[in] |
| PWM functionality duty cycle in percentage |
ReturnsSL_STATUS_OK if successful. Error code otherwise.
◆sl_bt_coex_set_directional_priority_pulse()#
sl_status_t sl_bt_coex_set_directional_priority_pulse | ( | uint8_t |
| ) |
Set Directional Priority Pulse Width.
Parameters
[in] |
| Directional priority pulse width in us |
ReturnsSL_STATUS_OK if successful. Error code otherwise.
◆sl_bt_coex_get_parameters()#
sl_status_t sl_bt_coex_get_parameters | ( | uint8_t * |
|
uint8_t * |
| ||
uint8_t * |
| ||
uint8_t * |
| ||
) |
Get the coexistence parameters.
Parameters
[out] |
| Coexistence priority threshold. Coexistence priority is toggled if priority is below this value. |
[out] |
| Coexistence request threshold. Coexistence request is toggled if priority is below this value. |
[out] |
| PWM functionality period length in 1 ms units |
[out] |
| PWM functionality duty cycle in percentage |
ReturnsSL_STATUS_OK if successful. Error code otherwise.
◆sl_bt_coex_get_counters()#
sl_status_t sl_bt_coex_get_counters | ( | uint8_t |
|
size_t |
| ||
size_t * |
| ||
uint8_t * |
| ||
) |
Read coexistence statistic counters from the device. Response contains the list of uint32 type counter values. Counters in the list are in following order: low priority requested, high priority requested, low priority denied, high priority denied, low-priority TX aborted, and high-priority TX aborted. Passing a non-zero value also resets counters.
Parameters
[in] |
| Reset counters if parameter value is not zero. |
[in] |
| Size of output buffer passed in |
[out] |
| On return, set to the length of output data written to |
[out] |
| Coexistence statistic counters |
ReturnsSL_STATUS_OK if successful. Error code otherwise.