ESL Tag User Defined Display Driver#
This component provides skeleton code for a user defined display driver - to be filled in with actual low level driver code for driving any arbitrary ESL Tag display type. See the Doxygen comments in the header file on usage. This is a Custom-Code component.
Functions#
Function Documentation#
esl_user_display_init#
sl_status_t esl_user_display_init (int param_count,...)
[in] | param_count | Number of parameters following (mandatory, equals to 'ESL_DISPLAY_INIT_FUNC_PARAMETERS_COUNT' defined by esl_tag_display component. |
[in] | uint8_t type of the display index |
ESL Tag user defined display driver init function. Function naming is for reference, only - any arbitrary function naming can be used, freely. For more - and especially, different type of displays - there might be a good approach to implement more init functions, also. Then, these functions has to be assigned to the corresponding display during the esl_core_boot_event as follows:
sl_status_t void esl_core_boot_event(void)
{
sl_status_t sc;
esl_display_info_p info;
sc = esl_display_create(<user_display_witdth>,
<user_display_height>,
<user_display_type>,
&info);
app_assert_status(sc);
sc = esl_display_add(info,
<your_init_function>, // can be NULL if not needed
<your_write_function>); // mandatory!
app_assert_status(sc);
}
Note: please do not forget to add #include "esl_display.h", previously.
71
of file common/esl_tag_user_display_driver/inc/esl_tag_user_display_driver.h
esl_user_display_write#
sl_status_t esl_user_display_write (int param_count,...)
[in] | param_count | Number of parameters following (mandatory, equals to 'ESL_DISPLAY_WRITE_FUNC_PARAMETERS_COUNT' defined by esl_tag_display component. |
[in] | uint8_t type of the display index | |
[in] | image_index | uint8_t type of the image index |
ESL Tag display user defined driver write function. See the comments at esl_user_display_init function on naming and usage.
82
of file common/esl_tag_user_display_driver/inc/esl_tag_user_display_driver.h