Ambient light and UV index sensor#

Ambient light and UV index sensor driver abstraction designed for Thunderboard.

Functions#

sl_status_t
sl_status_t
sl_sensor_light_get(float *lux, float *uvi)

Function Documentation#

sl_sensor_light_init#

sl_status_t sl_sensor_light_init (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Initialize ambient light and UV index sensor.

Note

  • With certain boards (e.g. 4166A, 4184A), using this initialization function enables other sensors, because they're on the same enable pin. Please take that into account when using this function.

Returns

  • Status of the operation.


sl_sensor_light_deinit#

void sl_sensor_light_deinit (void )
Parameters
TypeDirectionArgument NameDescription
voidN/A

Deinitialize ambient light and UV index sensor.

Warnings

  • With certain boards (e.g. 4166A, 4184A), using this deinitialization function disables other sensors, because they're on the same enable pin. Please use with caution.


sl_sensor_light_get#

sl_status_t sl_sensor_light_get (float * lux, float * uvi)
Parameters
TypeDirectionArgument NameDescription
float *[out]lux

Ambient light illuminance (in lux).

float *[out]uvi

UV index.

Getter for ambient light and UV index sensor measurement data. Returns

  • Status of the operation.


Macro Definition Documentation#

SENSOR_LIGHT_POSITIVE_TOLERANCE#

#define SENSOR_LIGHT_POSITIVE_TOLERANCE
Value:
0

SENSOR_LIGHT_NEGATIVE_TOLERANCE#

#define SENSOR_LIGHT_NEGATIVE_TOLERANCE
Value:
0

SENSOR_LIGHT_SAMPLING_FUNCTION#

#define SENSOR_LIGHT_SAMPLING_FUNCTION
Value:
SAMPLING_UNSPECIFIED

SENSOR_LIGHT_MEASUREMENT_PERIOD#

#define SENSOR_LIGHT_MEASUREMENT_PERIOD
Value:
0

SENSOR_LIGHT_UPDATE_INTERVAL#

#define SENSOR_LIGHT_UPDATE_INTERVAL
Value:
0