Constant Tone Extension GATT Service (Connectionless)#
Constant Tone Extension GATT Service reference implementation for periodic advertising. Limitations:
The Bluetooth SIG specifies to maintain a list about the characteristic values for each client and take the largest/smallest value. Instead of this, the latest valid value will take effect.
The Advertising Constant Tone Extension Transmit Duration characteristic is not implemented.
The AoD mode parameters are configured globally in the Constant Tone Extension GATT Service (Connection) component.
Macros#
Macro Definition Documentation#
SL_GATT_SERVICE_CTE_CONNECTIONLESS_ADV_INTERVAL#
#define SL_GATT_SERVICE_CTE_CONNECTIONLESS_ADV_INTERVALValue:
16
SL_GATT_SERVICE_CTE_CONNECTIONLESS_MIN_LEN#
#define SL_GATT_SERVICE_CTE_CONNECTIONLESS_MIN_LENValue:
20
SL_GATT_SERVICE_CTE_CONNECTIONLESS_MIN_TX_COUNT#
#define SL_GATT_SERVICE_CTE_CONNECTIONLESS_MIN_TX_COUNTValue:
1
SL_GATT_SERVICE_CTE_CONNECTIONLESS_ADV_CTE_PHY#
#define SL_GATT_SERVICE_CTE_CONNECTIONLESS_ADV_CTE_PHYValue:
0