Environment Sensing - Air Pressure GATT Service#

Provides air pressure sensor data in GATT characteristics. Designed for the Thunderboard smartphone app.

Functions#

void
sl_status_t

Macros#

Function Documentation#

sl_gatt_service_pressure_on_event#

void sl_gatt_service_pressure_on_event (sl_bt_msg_t * evt)
Parameters
TypeDirectionArgument NameDescription
sl_bt_msg_t *[in]evt

Event coming from the Bluetooth stack.

Bluetooth stack event handler.


sl_gatt_service_pressure_get#

sl_status_t sl_gatt_service_pressure_get (float * pressure)
Parameters
TypeDirectionArgument NameDescription
float *[out]pressure

Barometric pressure (in millibars).

Getter for Pressure characteristic value. Returns

  • Status of the operation.

Note

  • To be implemented in user code.


Macro Definition Documentation#

SL_GATT_SERVICE_PRESSURE_INVALID#

#define SL_GATT_SERVICE_PRESSURE_INVALID
Value:
0xFFFFFFFF