Filter Accept List#

Filter Accept List.

Provides support for adding and removing devices from the Filter Accept List in the Bluetooth controller.

The Filter Accept List allows filtering transmissions from other Bluetooth devices so that the local device only receives/accepts transmissions from the devices that it's interested in or wants to communicate with. Operations that support filtering provide a means to control how the Filter Accept List is used:

Functions#

sl_status_t
sl_status_t
sl_bt_accept_list_add_device_by_address(bd_addr address, uint8_t address_type)
sl_status_t
sl_status_t
sl_bt_accept_list_remove_device_by_address(bd_addr address, uint8_t address_type)

Macros#

#define
sl_bt_cmd_accept_list_add_device_by_bonding_id 0x005e0020
#define
sl_bt_cmd_accept_list_add_device_by_address_id 0x015e0020
#define
sl_bt_cmd_accept_list_remove_device_by_bonding_id 0x025e0020
#define
sl_bt_cmd_accept_list_remove_device_by_address_id 0x035e0020
#define
sl_bt_cmd_accept_list_remove_all_devices_id 0x045e0020
#define
sl_bt_rsp_accept_list_add_device_by_bonding_id 0x005e0020
#define
sl_bt_rsp_accept_list_add_device_by_address_id 0x015e0020
#define
sl_bt_rsp_accept_list_remove_device_by_bonding_id 0x025e0020
#define
sl_bt_rsp_accept_list_remove_device_by_address_id 0x035e0020
#define
sl_bt_rsp_accept_list_remove_all_devices_id 0x045e0020

Function Documentation#

sl_bt_accept_list_add_device_by_bonding#

sl_status_t sl_bt_accept_list_add_device_by_bonding (uint32_t bonding)
Parameters
TypeDirectionArgument NameDescription
uint32_t[in]bonding

The bonding handle

Add a device to the Filter Accept List based on its bonding handle.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 11650 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_accept_list_add_device_by_address#

sl_status_t sl_bt_accept_list_add_device_by_address (bd_addr address, uint8_t address_type)
Parameters
TypeDirectionArgument NameDescription
bd_addr[in]address

Bluetooth address of the peer device

uint8_t[in]address_type

Enum sl_bt_gap_address_type_t. The peer device address type. Values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_anonymous_address (0xff): Anonymous address. A Filter Accept List entry with this type matches all advertisements sent with no address.

Add a device to the Filter Accept List based on its identity address.

Use the special address type sl_bt_gap_anonymous_address to add an entry that matches all advertisements sent with no address.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 11671 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_accept_list_remove_device_by_bonding#

sl_status_t sl_bt_accept_list_remove_device_by_bonding (uint32_t bonding)
Parameters
TypeDirectionArgument NameDescription
uint32_t[in]bonding

The bonding handle

Remove a device from the Filter Accept List based on its bonding handle.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 11683 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_accept_list_remove_device_by_address#

sl_status_t sl_bt_accept_list_remove_device_by_address (bd_addr address, uint8_t address_type)
Parameters
TypeDirectionArgument NameDescription
bd_addr[in]address

Bluetooth address of the peer device

uint8_t[in]address_type

Enum sl_bt_gap_address_type_t. The peer device address type. Values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_anonymous_address (0xff): Anonymous address. A Filter Accept List entry with this type matches all advertisements sent with no address.

Remove a device from the Filter Accept List based on its identity address.

Use the special address type sl_bt_gap_anonymous_address to remove an entry that matches all advertisements sent with no address.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 11704 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h

sl_bt_accept_list_remove_all_devices#

sl_status_t sl_bt_accept_list_remove_all_devices ()

Remove all devices from the Filter Accept List.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 11715 of file /mnt/raid/workspaces/ws.vHmYkJajL/overlay/gsdk/protocol/bluetooth/build_debug/bt_api/sw/bgapi/inc/sl_bt_api.h