Modules#

sl_bt_evt_cs_security_enable_complete

sl_bt_evt_cs_config_complete

sl_bt_evt_cs_procedure_enable_complete

sl_bt_evt_cs_result

Accurate Bluetooth Ranging#

Accurate Bluetooth Ranging.

This class provides commands and events for Accurate Bluetooth Ranging (ABR) between Bluetooth devices.

Enumerations#

enum
sl_bt_cs_role_initiator = 0x0
sl_bt_cs_role_reflector = 0x1
}

Specifies the role for the device during ABR procedure.

enum
sl_bt_cs_role_status_disable = 0x0
sl_bt_cs_role_status_enable = 0x1
}

Defines the status of a given role for an ABR capable device.

enum
sl_bt_cs_companion_signal_status_disable = 0x0
sl_bt_cs_companion_signal_status_enable = 0x1
}

Defines the status of a companion signal.

enum
sl_bt_cs_procedure_state_disabled = 0x0
sl_bt_cs_procedure_state_enabled = 0x1
}

Defines the ABR procedure state for the device.

enum
sl_bt_cs_mode_calibration = 0x0
sl_bt_cs_mode_rtt = 0x1
sl_bt_cs_mode_pbr = 0x2
sl_bt_cs_mode_pbr_and_rtt = 0x3
}

Defines the different modes for ABR steps.

enum
sl_bt_cs_rtt_type_coarse = 0x0
sl_bt_cs_rtt_type_fractional_96_bit_sounding = 0x2
}

Defines the Round Trip Time (RTT) payload types used during the ABR sequence.

enum
sl_bt_cs_channel_selection_algorithm_3b = 0x0
sl_bt_cs_channel_selection_algorithm_3c = 0x1
sl_bt_cs_channel_selection_algorithm_user_shape_interleaved = 0x2
}

Specifies the ABR channel selection algorithms.

enum
sl_bt_cs_ch3c_shape_hat = 0x0
sl_bt_cs_chc3_shape_interleaved = 0x1
}

Specifies the ch3c shapes.

enum
sl_bt_cs_done_status_complete = 0x0
sl_bt_cs_done_status_partial_results_continue = 0x1
sl_bt_cs_done_status_current_aborted = 0xfe
sl_bt_cs_done_status_all_aborted = 0xff
}

Describes the current status of the procedure or subevents.

enum
sl_bt_cs_abort_reason_no_abort = 0x0
sl_bt_cs_abort_reason_host_request = 0x1
sl_bt_cs_abort_reason_insufficient_channels = 0x2
sl_bt_cs_abort_reason_no_map_update = 0x3
sl_bt_cs_abort_reason_unspecified = 0xf
}

Describes the abort reasons for ABR procedures and subevents and is represented by 4 bits in a byte.

enum
sl_bt_cs_config_state_removed = 0x0
sl_bt_cs_config_state_created = 0x1
}

Specifies the role for the device during ABR procedure.

Functions#

sl_status_t
sl_bt_cs_security_enable(uint8_t connection)
sl_status_t
sl_bt_cs_set_default_settings(uint8_t connection, uint8_t initiator_status, uint8_t reflector_status, uint8_t antenna_identifier, int8_t max_tx_power)
sl_status_t
sl_bt_cs_create_config(uint8_t connection, uint8_t config_id, uint8_t create_context, uint8_t main_mode_type, uint8_t sub_mode_type, uint8_t min_main_mode_steps, uint8_t max_main_mode_steps, uint8_t main_mode_repetition, uint8_t mode_calibration_steps, uint8_t role, uint8_t rtt_type, uint8_t cs_sync_phy, const sl_bt_cs_channel_map_t *channel_map, uint8_t channel_map_repetition, uint8_t channel_selection_type, uint8_t ch3c_shape, uint8_t ch3c_jump, uint8_t companion_signal_state)
sl_status_t
sl_bt_cs_remove_config(uint8_t connection, uint8_t config_id)
sl_status_t
sl_bt_cs_set_channel_classification(const sl_bt_cs_channel_map_t *channel_map)
sl_status_t
sl_bt_cs_set_procedure_parameters(uint8_t connection, uint8_t config_id, uint16_t max_procedure_len, uint16_t min_procedure_interval, uint16_t max_procedure_interval, uint16_t max_procedure_count, uint32_t min_subevent_len, uint32_t max_subevent_len, uint8_t tone_antenna_config_selection, uint8_t phy, int8_t tx_pwr_delta, uint8_t preferred_peer_antenna)
sl_status_t
sl_bt_cs_procedure_enable(uint8_t connection, uint8_t enable, uint8_t config_id)
sl_status_t
sl_bt_cs_set_antenna_configuration(size_t antenna_element_offset_len, const uint8_t *antenna_element_offset)

Enumeration Documentation#

sl_bt_cs_role_t#

sl_bt_cs_role_t

Specifies the role for the device during ABR procedure.

Enumerator
sl_bt_cs_role_initiator

(0x0) The device will initiate the procedure

sl_bt_cs_role_reflector

(0x1) The device will reciprocate transmission


sl_bt_cs_role_status_t#

sl_bt_cs_role_status_t

Defines the status of a given role for an ABR capable device.

Enumerator
sl_bt_cs_role_status_disable

(0x0) The given role is disabled

sl_bt_cs_role_status_enable

(0x1) The given role is enabled


sl_bt_cs_companion_signal_status_t#

sl_bt_cs_companion_signal_status_t

Defines the status of a companion signal.

Enumerator
sl_bt_cs_companion_signal_status_disable

(0x0) The companion signal is disabled

sl_bt_cs_companion_signal_status_enable

(0x1) The companion signal is enabled


sl_bt_cs_procedure_state_t#

sl_bt_cs_procedure_state_t

Defines the ABR procedure state for the device.

Enumerator
sl_bt_cs_procedure_state_disabled

(0x0) ABR procedures are disabled

sl_bt_cs_procedure_state_enabled

(0x1) ABR procedures are enabled


sl_bt_cs_mode_t#

sl_bt_cs_mode_t

Defines the different modes for ABR steps.

Enumerator
sl_bt_cs_mode_calibration

(0x0) Frequency offset and timing calibration measurement

sl_bt_cs_mode_rtt

(0x1) Round Trip Time (RTT) measurement

sl_bt_cs_mode_pbr

(0x2) Phase-Based Ranging (PBR) measurement

sl_bt_cs_mode_pbr_and_rtt

(0x3) PBR and RTT measurement


sl_bt_cs_rtt_type_t#

sl_bt_cs_rtt_type_t

Defines the Round Trip Time (RTT) payload types used during the ABR sequence.

Enumerator
sl_bt_cs_rtt_type_coarse

(0x0) RTT Coarse

sl_bt_cs_rtt_type_fractional_96_bit_sounding

(0x2) RTT Fractional with 96-bit Sounding Sequence


sl_bt_cs_channel_selection_algorithm_t#

sl_bt_cs_channel_selection_algorithm_t

Specifies the ABR channel selection algorithms.

Enumerator
sl_bt_cs_channel_selection_algorithm_3b

(0x0) Use Channel Selection Algorithm #3b for non-mode 0 ABR steps

sl_bt_cs_channel_selection_algorithm_3c

(0x1) Use Channel Selection Algorithm #3c for non-mode 0 ABR steps

sl_bt_cs_channel_selection_algorithm_user_shape_interleaved

(0x2) Use Interleaved shape for user specified channel sequence


sl_bt_cs_ch3c_shape_t#

sl_bt_cs_ch3c_shape_t

Specifies the ch3c shapes.

Enumerator
sl_bt_cs_ch3c_shape_hat

(0x0) Use Hat shape for user specified channel sequence

sl_bt_cs_chc3_shape_interleaved

(0x1) Use Interleaved shape for user specified channel sequence


sl_bt_cs_done_status_t#

sl_bt_cs_done_status_t

Describes the current status of the procedure or subevents.

Enumerator
sl_bt_cs_done_status_complete

(0x0) All results complete for the ABR procedure or subevent

sl_bt_cs_done_status_partial_results_continue

(0x1) Partial results with more to follow

sl_bt_cs_done_status_current_aborted

(0xfe) Current ABR procedure or subevent aborted

sl_bt_cs_done_status_all_aborted

(0xff) Current and all subsequent subevents in the procedure aborted


sl_bt_cs_abort_reason_t#

sl_bt_cs_abort_reason_t

Describes the abort reasons for ABR procedures and subevents and is represented by 4 bits in a byte.

Enumerator
sl_bt_cs_abort_reason_no_abort

(0x0) Not aborted

sl_bt_cs_abort_reason_host_request

(0x1) Local or remote host request

sl_bt_cs_abort_reason_insufficient_channels

(0x2) Filtered channel has less than 15 channels

sl_bt_cs_abort_reason_no_map_update

(0x3) Channel map update instant has passed

sl_bt_cs_abort_reason_unspecified

(0xf) Unspecified reasons for abortion


sl_bt_cs_config_state_t#

sl_bt_cs_config_state_t

Specifies the role for the device during ABR procedure.

Enumerator
sl_bt_cs_config_state_removed

(0x0) The ABR device configuration is removed

sl_bt_cs_config_state_created

(0x1) The ABR device configuration is created


Function Documentation#

sl_bt_cs_security_enable#

sl_status_t sl_bt_cs_security_enable (uint8_t connection)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection handle

Start or restart ABR security start procedure for the specified connection.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_bt_cs_set_default_settings#

sl_status_t sl_bt_cs_set_default_settings (uint8_t connection, uint8_t initiator_status, uint8_t reflector_status, uint8_t antenna_identifier, int8_t max_tx_power)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection handle

uint8_t[in]initiator_status

Enum sl_bt_cs_role_status_t. Enable or disable status of the Initiator role. Values:

  • sl_bt_cs_role_status_disable (0x0): The given role is disabled

  • sl_bt_cs_role_status_enable (0x1): The given role is enabled

uint8_t[in]reflector_status

Enum sl_bt_cs_role_status_t. Enable or disable status of the Reflector role. Values:

  • sl_bt_cs_role_status_disable (0x0): The given role is disabled

  • sl_bt_cs_role_status_enable (0x1): The given role is enabled

uint8_t[in]antenna_identifier

Antenna identifier to be used for ABR sync packets.

  • Range: 1 to 4

int8_t[in]max_tx_power

Maximum transmit power level to be used in all ABR transmissions. Units: dBm.

  • Range: -127 to +20

Set the default ABR settings for the specified connection. By default, all roles are disabled and the antenna is set to 1.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_cs_create_config#

sl_status_t sl_bt_cs_create_config (uint8_t connection, uint8_t config_id, uint8_t create_context, uint8_t main_mode_type, uint8_t sub_mode_type, uint8_t min_main_mode_steps, uint8_t max_main_mode_steps, uint8_t main_mode_repetition, uint8_t mode_calibration_steps, uint8_t role, uint8_t rtt_type, uint8_t cs_sync_phy, const sl_bt_cs_channel_map_t * channel_map, uint8_t channel_map_repetition, uint8_t channel_selection_type, uint8_t ch3c_shape, uint8_t ch3c_jump, uint8_t companion_signal_state)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

The connection handle

uint8_t[in]config_id

ABR configuration identifier.

  • Range: 0 to 3

uint8_t[in]create_context

Defines in which device the created configuration will be written

  • Value: 0x00. Write ABR configuration in the local controller only

  • Value: 0x01. Write ABR configuration in both the local and remote controller using a configuration procedure

uint8_t[in]main_mode_type

Enum sl_bt_cs_mode_t. Main mode type. Values:

  • sl_bt_cs_mode_calibration (0x0): Frequency offset and timing calibration measurement

  • sl_bt_cs_mode_rtt (0x1): Round Trip Time (RTT) measurement

  • sl_bt_cs_mode_pbr (0x2): Phase-Based Ranging (PBR) measurement

  • sl_bt_cs_mode_pbr_and_rtt (0x3): PBR and RTT measurement

uint8_t[in]sub_mode_type

Enum sl_bt_cs_mode_t. Sub mode type. Values:

  • sl_bt_cs_mode_calibration (0x0): Frequency offset and timing calibration measurement

  • sl_bt_cs_mode_rtt (0x1): Round Trip Time (RTT) measurement

  • sl_bt_cs_mode_pbr (0x2): Phase-Based Ranging (PBR) measurement

  • sl_bt_cs_mode_pbr_and_rtt (0x3): PBR and RTT measurement

uint8_t[in]min_main_mode_steps

Minimum number of ABR main mode steps to be executed prior to a sub mode step.

  • Range: 1 to 160

uint8_t[in]max_main_mode_steps

Maximum number of ABR main mode steps to be executed prior to a sub mode step.

  • Range: 1 to 160

uint8_t[in]main_mode_repetition

Number of main mode steps taken from the end of the last ABR subevent to be repeated at the beginning of the current ABR subevent directly after the value r last Mode 0 step of that event.

  • Range: 0 to 3

uint8_t[in]mode_calibration_steps

Number of Mode 0 steps to be included at the beginning of the test ABR subevent

  • Range: 1 to 3

uint8_t[in]role

Enum sl_bt_cs_role_t. Device's role during the ABR procedure Values:

  • sl_bt_cs_role_initiator (0x0): The device will initiate the procedure

  • sl_bt_cs_role_reflector (0x1): The device will reciprocate transmission

uint8_t[in]rtt_type

Enum sl_bt_cs_rtt_type_t. RTT payload type used in the ABR procedure Values:

  • sl_bt_cs_rtt_type_coarse (0x0): RTT Coarse

  • sl_bt_cs_rtt_type_fractional_96_bit_sounding (0x2): RTT Fractional with 96-bit Sounding Sequence

uint8_t[in]cs_sync_phy

Enum sl_bt_gap_phy_t. Used PHY for ABR SYNC exchanges during a procedure Values:

  • sl_bt_gap_phy_1m (0x1): 1M PHY

const sl_bt_cs_channel_map_t *[in]channel_map

A fixed length byte array of 10 bytes consisting of 79 1-bit fields.

The nth such field (in the range 0 to 78) contains the value for the ABR channel index n.

  • Bit value 0: Channel n is disabled

  • Bit value 1: Channel n is enabled

The rest of most significant bits are reserved for future use and must be set to 0. Channels n = 0, 1, 23, 24, 25, 77 and 78 shall be ignored and not used for ABR. At least 15 channels shall be marked as used.

uint8_t[in]channel_map_repetition

Number of times the channel_map field will be cycled through for non-Mode 0 steps within an ABR procedure.

  • Range: 0x01 to 0xFF

uint8_t[in]channel_selection_type

Enum sl_bt_cs_channel_selection_algorithm_t. Channel selection algorithm Values:

  • sl_bt_cs_channel_selection_algorithm_3b (0x0): Use Channel Selection Algorithm #3b for non-mode 0 ABR steps

  • sl_bt_cs_channel_selection_algorithm_3c (0x1): Use Channel Selection Algorithm #3c for non-mode 0 ABR steps

  • sl_bt_cs_channel_selection_algorithm_user_shape_interleaved (0x2): Use Interleaved shape for user specified channel sequence

uint8_t[in]ch3c_shape

Enum sl_bt_cs_ch3c_shape_t. Ch3c shape Values:

  • sl_bt_cs_ch3c_shape_hat (0x0): Use Hat shape for user specified channel sequence

  • sl_bt_cs_chc3_shape_interleaved (0x1): Use Interleaved shape for user specified channel sequence

uint8_t[in]ch3c_jump

Number of channels skipped in each rising and falling sequence.

  • Range: 2 to 8

uint8_t[in]companion_signal_state

Enum sl_bt_cs_companion_signal_status_t. Companion device's signal status Values:

  • sl_bt_cs_companion_signal_status_disable (0x0): The companion signal is disabled

  • sl_bt_cs_companion_signal_status_enable (0x1): The companion signal is enabled

Create a new ABR configuration in the local and remote controller. The role used in this command must be enabled prior to issuing this command using sl_bt_cs_set_default_settings command.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_bt_cs_remove_config#

sl_status_t sl_bt_cs_remove_config (uint8_t connection, uint8_t config_id)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection handle

uint8_t[in]config_id

ABR configuration identifier

  • Range: 0 to 3

Remove an ABR configuration from the local controller.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_bt_cs_set_channel_classification#

sl_status_t sl_bt_cs_set_channel_classification (const sl_bt_cs_channel_map_t * channel_map)
Parameters
TypeDirectionArgument NameDescription
const sl_bt_cs_channel_map_t *[in]channel_map

A fixed length byte array of 10 bytes consisting of 79 1-bit fields.

The nth field (in the range 0 to 78) contains the value for the link layer channel index n.

  • Bit value 0: Channel n is disabled.

  • Bit value 1: Channel n is enabled.

The rest of most significant bits are reserved for future use and must be set to 0. Channels n = 0, 1, 23, 24, 25, 77 and 78 shall be ignored and not used for ABR.

Update the channel classification for ABR. This classification persists until overwritten with a subsequent command or until the system is reset.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_cs_set_procedure_parameters#

sl_status_t sl_bt_cs_set_procedure_parameters (uint8_t connection, uint8_t config_id, uint16_t max_procedure_len, uint16_t min_procedure_interval, uint16_t max_procedure_interval, uint16_t max_procedure_count, uint32_t min_subevent_len, uint32_t max_subevent_len, uint8_t tone_antenna_config_selection, uint8_t phy, int8_t tx_pwr_delta, uint8_t preferred_peer_antenna)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

The connection handle

uint8_t[in]config_id

ABR configuration identifier.

  • Range: 0 to 3.

uint16_t[in]max_procedure_len

Maximum duration for each measurement procedure. Value in units of 0.625 ms.

  • Range: 0x0001 to 0xFFFF.

  • Time: N x 0.625ms. N being the input.

  • Time range: 0.625 ms to 40.959375 s.

uint16_t[in]min_procedure_interval

Minimum duration in number of connection events between consecutive measurement procedure.

  • Range: 0x01 to 0xFFFF.

uint16_t[in]max_procedure_interval

Maximum duration in number of connection events between consecutive measurement procedure.

  • Range: 0x01 to 0xFFFF.

uint16_t[in]max_procedure_count

Maximum number of ABR procedures to be scheduled

  • Range: 0x01 to 0xFFFF: Maximum number of procedures to be scheduled.

  • Value: 0x00. Procedures to continue until disabled.

uint32_t[in]min_subevent_len

Minimum suggested duration for each ABR subevent. Units: microseconds.

  • Range: 0x01 to 0xFFFFFF

  • Time range: 1250 us to 4s

uint32_t[in]max_subevent_len

Maximum suggested duration for each ABR subevent. Units: microseconds.

  • Range: 0x01 to 0xFFFFFF

  • Time range: 1250 us to 4s

uint8_t[in]tone_antenna_config_selection

Antenna configuration index

  • Range: 0 to 7

uint8_t[in]phy

Enum sl_bt_gap_phy_t. PHY on which the ABR transmission will take place Values:

  • sl_bt_gap_phy_1m (0x1): 1M PHY

  • sl_bt_gap_phy_2m (0x2): 2M PHY

  • sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8) or 500k (S=2)

  • sl_bt_gap_phy_any (0xff): Any PHYs the device supports

int8_t[in]tx_pwr_delta

Transmit power delta. Units: dB.

  • Value: 0x80. Host does not have a recommendation for transmit power delta

uint8_t[in]preferred_peer_antenna

Preferred peer-ordered antenna elements to be used by the remote device for the antenna configuration denoted by the tone antenna config selection.

  • Bit 0: Use first ordered antenna element

  • Bit 1: Use second ordered antenna element

  • Bit 2: Use third ordered antenna element

  • Bit 3: Use fourth ordered antenna element

Set the parameters for scheduling ABR procedures with the remote device.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


sl_bt_cs_procedure_enable#

sl_status_t sl_bt_cs_procedure_enable (uint8_t connection, uint8_t enable, uint8_t config_id)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

The connection handle

uint8_t[in]enable

Enum sl_bt_cs_procedure_state_t. Enabled or disabled ABR procedure state. Values:

  • sl_bt_cs_procedure_state_disabled (0x0): ABR procedures are disabled

  • sl_bt_cs_procedure_state_enabled (0x1): ABR procedures are enabled

uint8_t[in]config_id

ABR configuration identifier

Enable or disable scheduling ABR procedures with the remote device.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


sl_bt_cs_set_antenna_configuration#

sl_status_t sl_bt_cs_set_antenna_configuration (size_t antenna_element_offset_len, const uint8_t * antenna_element_offset)
Parameters
TypeDirectionArgument NameDescription
size_t[in]antenna_element_offset_len

Length of data in antenna_element_offset

const uint8_t *[in]antenna_element_offset

Offset of each antenna, each element is a signed 16-bit integer stored in two consecutive bytes in little-endian order. Units: 1 cm.

Set the antenna configuration for the ABR feature.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Macro Definition Documentation#

sl_bt_cmd_cs_security_enable_id#

#define sl_bt_cmd_cs_security_enable_id
Value:
0x00590020

sl_bt_cmd_cs_set_default_settings_id#

#define sl_bt_cmd_cs_set_default_settings_id
Value:
0x01590020

sl_bt_cmd_cs_create_config_id#

#define sl_bt_cmd_cs_create_config_id
Value:
0x02590020

sl_bt_cmd_cs_remove_config_id#

#define sl_bt_cmd_cs_remove_config_id
Value:
0x03590020

sl_bt_cmd_cs_set_channel_classification_id#

#define sl_bt_cmd_cs_set_channel_classification_id
Value:
0x04590020

sl_bt_cmd_cs_set_procedure_parameters_id#

#define sl_bt_cmd_cs_set_procedure_parameters_id
Value:
0x05590020

sl_bt_cmd_cs_procedure_enable_id#

#define sl_bt_cmd_cs_procedure_enable_id
Value:
0x06590020

sl_bt_cmd_cs_set_antenna_configuration_id#

#define sl_bt_cmd_cs_set_antenna_configuration_id
Value:
0x07590020

sl_bt_rsp_cs_security_enable_id#

#define sl_bt_rsp_cs_security_enable_id
Value:
0x00590020

sl_bt_rsp_cs_set_default_settings_id#

#define sl_bt_rsp_cs_set_default_settings_id
Value:
0x01590020

sl_bt_rsp_cs_create_config_id#

#define sl_bt_rsp_cs_create_config_id
Value:
0x02590020

sl_bt_rsp_cs_remove_config_id#

#define sl_bt_rsp_cs_remove_config_id
Value:
0x03590020

sl_bt_rsp_cs_set_channel_classification_id#

#define sl_bt_rsp_cs_set_channel_classification_id
Value:
0x04590020

sl_bt_rsp_cs_set_procedure_parameters_id#

#define sl_bt_rsp_cs_set_procedure_parameters_id
Value:
0x05590020

sl_bt_rsp_cs_procedure_enable_id#

#define sl_bt_rsp_cs_procedure_enable_id
Value:
0x06590020

sl_bt_rsp_cs_set_antenna_configuration_id#

#define sl_bt_rsp_cs_set_antenna_configuration_id
Value:
0x07590020