Battery GATT Service#

Provides battery sensor data in GATT characteristics. Designed for the Thunderboard smartphone app.

Function Documentation#

sl_gatt_service_battery_on_event#

void sl_gatt_service_battery_on_event (sl_bt_msg_t * evt)
Parameters
[in]evt

Event coming from the Bluetooth stack.

Bluetooth stack event handler.


Definition at line 45 of file common/gatt_service_battery/sl_gatt_service_battery.h

sl_gatt_service_battery_get_level#

uint8_t sl_gatt_service_battery_get_level (void )
Parameters
N/A

Getter for Battery Level characteristic value. Returns

  • Battery charge level percent (0..100).

Note

  • To be implemented in user code.


Definition at line 52 of file common/gatt_service_battery/sl_gatt_service_battery.h

sl_gatt_service_battery_get_type#

uint8_t sl_gatt_service_battery_get_type (void )
Parameters
N/A

Getter for Power Source characteristic value. Returns

  • Power source type represented as an integer.

Note

  • To be implemented in user code.


Definition at line 59 of file common/gatt_service_battery/sl_gatt_service_battery.h