Advertiser PAST#

Advertiser PAST.

Transfer the synchronization information of a local active periodic advertising set to a remote device using Periodic Advertising Synchronization Transfer (PAST) over a connection.

Functions#

sl_status_t
sl_bt_advertiser_past_transfer(uint8_t connection, uint16_t service_data, uint8_t advertising_set)

Function Documentation#

sl_bt_advertiser_past_transfer#

sl_status_t sl_bt_advertiser_past_transfer (uint8_t connection, uint16_t service_data, uint8_t advertising_set)
Parameters
TypeDirectionArgument NameDescription
uint8_t[in]connection

Connection handle of the connection used to transmit the sync transfer

uint16_t[in]service_data

A value provided by the application for use by the peer device.

uint8_t[in]advertising_set

Handle of the periodic advertising set to transfer

Transfer the synchronization information of an advertising set that is actively performing periodic advertising.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Macro Definition Documentation#

sl_bt_cmd_advertiser_past_transfer_id#

#define sl_bt_cmd_advertiser_past_transfer_id
Value:
0x00520020

sl_bt_rsp_advertiser_past_transfer_id#

#define sl_bt_rsp_advertiser_past_transfer_id
Value:
0x00520020