Transmit Power Reporting Constants#
Constants in transmit power reporting
Macro Definition Documentation#
SL_BT_CONNECTION_TX_POWER_UNMANAGED#
#define SL_BT_CONNECTION_TX_POWER_UNMANAGEDValue:
0x7e
Remote device is not managing power levels.
Definition at line
6486
of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
SL_BT_CONNECTION_TX_POWER_UNAVAILABLE
#define SL_BT_CONNECTION_TX_POWER_UNAVAILABLEValue:
0x7f
Transmit power level is not available.
Definition at line
6489
of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
SL_BT_CONNECTION_TX_POWER_CHANGE_UNAVAILABLE
#define SL_BT_CONNECTION_TX_POWER_CHANGE_UNAVAILABLEValue:
0x7f
Change is not available or is out of range.
Definition at line
6492
of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h