Data structure of the scan_request event.
Public Attribute Documentation#
handle#
uint8_t sl_bt_evt_advertiser_scan_request_s::handle
Advertising set handle where the scan request was received
2151
of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
address#
bd_addr sl_bt_evt_advertiser_scan_request_s::address
Bluetooth address of the scanner
2153
of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
address_type#
uint8_t sl_bt_evt_advertiser_scan_request_s::address_type
Enum sl_bt_gap_address_type_t.
Scanner address type.
If the application does not include the bluetooth_feature_use_accurate_api_address_types component, address_type
uses the following values:
0: Public address
1: Random address
If the application includes the bluetooth_feature_use_accurate_api_address_types component, address_type
uses enum sl_bt_gap_address_type_t values:
sl_bt_gap_public_address (0x0): Public device address
sl_bt_gap_static_address (0x1): Static device address
sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address
sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address
sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA)
sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA)
2154
of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
bonding#
uint8_t sl_bt_evt_advertiser_scan_request_s::bonding
Bonding handle if the remote scanning device has previously bonded with the local device. Values:
SL_BT_INVALID_BONDING_HANDLE (0xff): No bonding
Other: Bonding handle
2184
of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h