Data structure of the dtm_iq_report event.

Public Attributes#

uint16_t
uint8_t
int8_t
uint8_t

Public Attribute Documentation#

status#

uint16_t sl_bt_evt_cte_receiver_dtm_iq_report_s::status

Status of CTE IQ sampling


Definition at line 14462 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

channel#

uint8_t sl_bt_evt_cte_receiver_dtm_iq_report_s::channel

The channel on which the CTE packet was received


Definition at line 14463 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

rssi#

int8_t sl_bt_evt_cte_receiver_dtm_iq_report_s::rssi

RSSI in the received CTE packet. Unit: dBm


Definition at line 14465 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

rssi_antenna_id#

uint8_t sl_bt_evt_cte_receiver_dtm_iq_report_s::rssi_antenna_id

The ID of the antenna on which RSSI was measured


Definition at line 14466 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

cte_type#

uint8_t sl_bt_evt_cte_receiver_dtm_iq_report_s::cte_type

The CTE type

  • 0: AoA CTE response

  • 1: AoD CTE response with 1us slots

  • 2: AoD CTE response with 2us slots


Definition at line 14468 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

slot_durations#

uint8_t sl_bt_evt_cte_receiver_dtm_iq_report_s::slot_durations

Slot durations

  • 1: Switching and sampling slots are 1 us each

  • 2: Switching and sampling slots are 2 us each


Definition at line 14472 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

event_counter#

uint16_t sl_bt_evt_cte_receiver_dtm_iq_report_s::event_counter

The event counter of the periodic advertising train or the connection


Definition at line 14477 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

samples#

uint8array sl_bt_evt_cte_receiver_dtm_iq_report_s::samples

IQ samples of the received CTE packet. I and Q samples follow each other alternately (I, Q, I, Q, ...)


Definition at line 14479 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h