sl_bt_evt_gatt_descriptor#

Indicates that a GATT characteristic descriptor in the remote GATT database was discovered.

It is generated after issuing the sl_bt_gatt_discover_descriptors or sl_bt_gatt_discover_characteristic_descriptors command.

Modules#

sl_bt_evt_gatt_descriptor_s

Macros#

#define
sl_bt_evt_gatt_descriptor_id 0x030900a0

Identifier of the descriptor event.

Typedef Documentation#

sl_bt_evt_gatt_descriptor_t#

typedef struct sl_bt_evt_gatt_descriptor_s sl_bt_evt_gatt_descriptor_t

Definition at line 8093 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h