sl_bt_evt_gatt_server_attribute_value#

Indicates that the value of an attribute in the local GATT database was changed by a remote GATT client.

The parameter att_opcode describes which GATT procedure was used to change the value.

Modules#

sl_bt_evt_gatt_server_attribute_value_s

Macros#

#define
sl_bt_evt_gatt_server_attribute_value_id 0x000a00a0

Identifier of the attribute_value event.

Typedef Documentation#

sl_bt_evt_gatt_server_attribute_value_t#

typedef struct sl_bt_evt_gatt_server_attribute_value_s sl_bt_evt_gatt_server_attribute_value_t

Definition at line 9585 of file /mnt/raid/workspaces/ws.USsMlsi0G/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h