GAP#
GAP.
The commands and events in this class are related to the Generic Access Profile (GAP) in Bluetooth.
Enumerations#
These values define Bluetooth device address types. Commands and events that have Bluetooth device address parameters will specify which values are valid for that particular command or event.
Types of PHYs.
PHY types with coding schemes.
Types of channel selection algorithms in Link Layer.
Functions#
Macros#
Enumeration Documentation#
sl_bt_gap_address_type_t#
sl_bt_gap_address_type_t
These values define Bluetooth device address types. Commands and events that have Bluetooth device address parameters will specify which values are valid for that particular command or event.
If the application does not include the bluetooth_feature_use_accurate_api_address_types component, most Bluetooth commands and events use a coarse address type that only differentiates between a public address and any random address. When the application includes the bluetooth_feature_use_accurate_api_address_types component, Bluetooth commands and events that include an address type will systematically use values of this sl_bt_gap_address_type_t enumeration to indicate the accurate address type.
The values sl_bt_gap_public_address_resolved_from_rpa and sl_bt_gap_static_address_resolved_from_rpa are reported by the Bluetooth stack only when the application includes the bluetooth_feature_resolving_list component and the address was resolved in the Bluetooth controller. If the application uses these two types in input parameters, they are treated as synonyms of sl_bt_gap_public_address and sl_bt_gap_static_address, respectively.
| Enumerator | |
|---|---|
| sl_bt_gap_public_address | (0x0) Public device address |
| sl_bt_gap_static_address | (0x1) Static device address |
| sl_bt_gap_random_resolvable_address | (0x2) Resolvable private random address |
| sl_bt_gap_random_nonresolvable_address | (0x3) Non-resolvable private random address |
| sl_bt_gap_public_address_resolved_from_rpa | (0x4) Public identity address resolved from a resolvable private address (RPA) |
| sl_bt_gap_static_address_resolved_from_rpa | (0x5) Static identity address resolved from a resolvable private address (RPA) |
| sl_bt_gap_anonymous_address | (0xff) No address provided (anonymous advertising) |
sl_bt_gap_phy_t#
sl_bt_gap_phy_t
Types of PHYs.
| Enumerator | |
|---|---|
| sl_bt_gap_phy_1m | (0x1) 1M PHY |
| sl_bt_gap_phy_2m | (0x2) 2M PHY |
| sl_bt_gap_phy_coded | (0x4) Coded PHY, 125k (S=8) or 500k (S=2) |
| sl_bt_gap_phy_any | (0xff) Any PHYs the device supports |
sl_bt_gap_phy_coding_t#
sl_bt_gap_phy_coding_t
PHY types with coding schemes.
| Enumerator | |
|---|---|
| sl_bt_gap_phy_coding_1m_uncoded | (0x1) 1M PHY |
| sl_bt_gap_phy_coding_2m_uncoded | (0x2) 2M PHY |
| sl_bt_gap_phy_coding_125k_coded | (0x4) 125k Coded PHY (S=8) |
| sl_bt_gap_phy_coding_500k_coded | (0x8) 500k Coded PHY (S=2) |
sl_bt_gap_channel_selection_algorithm_t#
sl_bt_gap_channel_selection_algorithm_t
Types of channel selection algorithms in Link Layer.
| Enumerator | |
|---|---|
| sl_bt_gap_channel_selection_algorithm_1 | (0x0) Channel selection algorithm #1 |
| sl_bt_gap_channel_selection_algorithm_2 | (0x1) Channel selection algorithm #2 |
Function Documentation#
sl_bt_gap_set_privacy_mode#
sl_status_t sl_bt_gap_set_privacy_mode (uint8_t privacy, uint8_t interval)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | privacy | Values:
|
| uint8_t | [in] | interval | The minimum time interval between a private address change. This parameter is ignored if this command is issued to disable privacy mode. Values:
|
Enable or disable the privacy feature on all GAP roles. New privacy mode will take effect for advertising next time advertising is enabled, for scanning next time scanning is enabled, and for initiating on the next open connection command.
When privacy is enabled and the device is advertising or scanning, the stack will maintain a periodic timer with the specified time interval as a timeout value. At each timeout, the stack generates a new resolvable private address and uses it in scanning requests. For advertisers, the stack generates a new resolvable or non-resolvable private address and uses it in advertising data packets for each advertising set if its address is not application-managed, i.e., the address was not set by the application (with the sl_bt_advertiser_set_random_address command). The application is fully responsible for application-managed advertiser addresses. For an application-managed resolvable private address, the application should schedule periodic address updates for enhancing the privacy. It is recommended to use different schedules for different advertising sets.
Disabling the privacy during active advertising or scanning is not allowed.
By default, privacy feature is disabled.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_gap_set_data_channel_classification#
sl_status_t sl_bt_gap_set_data_channel_classification (size_t channel_map_len, const uint8_t * channel_map)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| size_t | [in] | channel_map_len | Length of data in |
| const uint8_t * | [in] | channel_map | 5 byte bit field in little endian format. Only the first 37 bits are used. Bit 0 of the first byte is channel 0, bit 0 of the second byte is channel 8, etc. Bits 37-39 are reserved for future use and must be set to 0. A channel is bad when its bit is 0. A channel is unknown when its bit is 1. At least two channels shall be marked as unknown. |
Specify a channel classification for data channels. This classification persists until overwritten with a subsequent command or until the system is reset. The value length of channel_map must be 5 bytes.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_gap_enable_whitelisting#
SL_BGAPI_DEPRECATED sl_status_t sl_bt_gap_enable_whitelisting (uint8_t enable)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | enable | 1 enable, 0 disable accept list filtering. |
Deprecated and replaced by functionality-specific settings provided by the bluetooth_feature_accept_list component. For advertising, use the command sl_bt_advertiser_configure and flags bits SL_BT_ADVERTISER_USE_FILTER_FOR_SCAN_REQUESTS and SL_BT_ADVERTISER_USE_FILTER_FOR_CONNECTION_REQUESTS to configure the advertising filter policy. For scanning, use the command sl_bt_scanner_set_parameters_and_filter to control the scanning filter policy.
Enable or disable accept list filtering. The setting will be effective the next time that scanning is enabled. Use command sl_bt_sm_add_to_whitelist to add devices to the accept list.
When the built-in bonding database (bluetooth_feature_builtin_bonding_database) is used, bonded devices are added into the accept list automatically by the stack. Note that the Bluetooth stack uses the built-in bonding database by default.
When the application specifically uses the external bonding database (bluetooth_feature_external_bonding_database), the application is fully responsible for managing the accept list using sl_bt_sm_add_to_whitelist and sl_bt_sm_delete_bondings commands.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_gap_set_identity_address#
sl_status_t sl_bt_gap_set_identity_address (bd_addr address, uint8_t addr_type)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bd_addr | [in] | address | The address in little endian format |
| uint8_t | [in] | addr_type | Enum sl_bt_gap_address_type_t. The address type. Values:
|
Set the device's Bluetooth identity address to be used in advertising, scanning, connection initiation, and identity address exchange in bonding. The address is stored in RAM only and does not change the identity address in persistent storage. The address can be a public device address or static device address. It will be effective immediately in the next advertising, scanning, connection initiation, and bonding. Error SL_STATUS_INVALID_PARAMETER is returned if the address does not conform to the Bluetooth specification.
Note that advertising sets that have own addresses set by sl_bt_advertiser_set_random_address are not affected by this command, i.e., they will continue to use their own user defined addresses.
Returns
SL_STATUS_OK if successful. Error code otherwise.