Synchronization#
Synchronization.
Provides the base functionality of periodic advertising synchronization. Use bluetooth_feature_sync_scanner and/or bluetooth_feature_past_receiver components to include the synchronization mechanisms that the application requires. Use bluetooth_feature_periodic_sync to include support for trains that do not have subevents or response slots, and/or bluetooth_feature_pawr_sync to include support for Periodic Advertising with Responses (PAwR) trains.
Some functionality in this class is considered deprecated and has been superseded by new classes. When one or more of bluetooth_feature_sync_scanner, bluetooth_feature_periodic_sync, or bluetooth_feature_pawr_sync components is included by the application, commands that have been superseded by the new classes are no longer available for use in the Synchronization class. Calling them will receive SL_STATUS_NOT_SUPPORTED error code. These commands are as follows:
See the command descriptions for the replacements.
Events that are deprecated and superseded by the new classes are no longer triggered by the Synchronization class if any of the new classes are included in the application. See event descriptions for the replacements.
Modules#
sl_bt_evt_sync_transfer_received
Enumerations#
Specifies the mode for periodic advertising reports.
These values indicate the advertiser clock accuracy in a periodic advertising synchronization.
Functions#
Macros#
Enumeration Documentation#
sl_bt_sync_reporting_mode_t#
sl_bt_sync_reporting_mode_t
Specifies the mode for periodic advertising reports.
| Enumerator | |
|---|---|
| sl_bt_sync_report_none | (0x0) Data received in periodic advertising trains is not reported to the application. |
| sl_bt_sync_report_all | (0x1) Data received in periodic advertising trains is reported to the application. |
sl_bt_sync_advertiser_clock_accuracy_t#
sl_bt_sync_advertiser_clock_accuracy_t
These values indicate the advertiser clock accuracy in a periodic advertising synchronization.
| Enumerator | |
|---|---|
| sl_bt_sync_clock_accuracy_500 | (0x1f4) Clock accuracy 500 ppm |
| sl_bt_sync_clock_accuracy_250 | (0xfa) Clock accuracy 250 ppm |
| sl_bt_sync_clock_accuracy_150 | (0x96) Clock accuracy 150 ppm |
| sl_bt_sync_clock_accuracy_100 | (0x64) Clock accuracy 100 ppm |
| sl_bt_sync_clock_accuracy_75 | (0x4b) Clock accuracy 75 ppm |
| sl_bt_sync_clock_accuracy_50 | (0x32) Clock accuracy 50 ppm |
| sl_bt_sync_clock_accuracy_30 | (0x1e) Clock accuracy 30 ppm |
| sl_bt_sync_clock_accuracy_20 | (0x14) Clock accuracy 20 ppm |
Function Documentation#
sl_bt_sync_set_parameters#
SL_BGAPI_DEPRECATED sl_status_t sl_bt_sync_set_parameters (uint16_t skip, uint16_t timeout, uint32_t flags)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | skip | The maximum number of periodic advertising packets that can be skipped after a successful receive.
|
| uint16_t | [in] | timeout | The maximum permitted time between successful receives. If this time is exceeded, synchronization is lost. Unit: 10 ms.
|
| uint32_t | [in] | flags | No flags defined currently |
Deprecated and replaced by sl_bt_sync_scanner_set_sync_parameters.
Configure periodic advertiser synchronization parameters. The specified parameters take effect immediately for all advertisers that have not already established synchronization.
The application should determine skip and timeout values based on the periodic advertising interval provided by the advertiser. Ensure that you use a long enough timeout to allow multiple receives. If skip and timeout are used, select appropriate values so that they allow a few receiving attempts. Periodic advertising intervals are reported in event sl_bt_evt_scanner_scan_report.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_sync_open#
SL_BGAPI_DEPRECATED sl_status_t sl_bt_sync_open (bd_addr address, uint8_t address_type, uint8_t adv_sid, uint16_t * sync)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| bd_addr | [in] | address | Address of the advertiser |
| uint8_t | [in] | address_type | Enum sl_bt_gap_address_type_t. Advertiser address type. If the application does not include the bluetooth_feature_use_accurate_api_address_types component,
If the application includes the bluetooth_feature_use_accurate_api_address_types component,
|
| uint8_t | [in] | adv_sid | Advertising set identifier |
| uint16_t * | [out] | sync | A handle that will be assigned to the periodic advertising synchronization after the synchronization is established. This handle is valid only if the result code of this response is SL_STATUS_OK. |
Deprecated and replaced by sl_bt_sync_scanner_open.
Start establishing synchronization with the specified periodic advertiser in parallel with other advertisers given in previous invocations of this command. The stack will internally enable scanning when needed so that synchronizations can occur. The scanning responses from the internal scanning are not passed to the application unless the application has also enabled scanning.
Advertisers that have not already synced before the invocation of this command will be synced using the skip and timeout values configured in the most recent invocation of command sl_bt_evt_scanner_scan_report.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_bt_evt_sync_opened - Triggered after the synchronization is established.
sl_bt_evt_sync_data - Indicates that a periodic advertisement packet is received.
sl_bt_evt_sync_closed - Triggered after periodic advertising synchronization was lost or explicitly closed, or a synchronization establishment procedure was canceled.
sl_bt_sync_set_reporting_mode#
sl_status_t sl_bt_sync_set_reporting_mode (uint16_t sync, uint8_t reporting_mode)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | sync | Periodic advertising synchronization handle |
| uint8_t | [in] | reporting_mode | Enum sl_bt_sync_reporting_mode_t. Specifies the mode for reporting data received in the periodic advertising train. Values:
|
Set data reporting mode of the periodic advertising synchronization.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_sync_update_sync_parameters#
sl_status_t sl_bt_sync_update_sync_parameters (uint16_t sync, uint16_t skip, uint16_t timeout)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | sync | Periodic advertising synchronization handle |
| uint16_t | [in] | skip | The maximum number of periodic advertising packets that can be skipped after a successful receive.
|
| uint16_t | [in] | timeout | The maximum permitted time between successful receives. If this time is exceeded, synchronization is lost. Unit: 10 ms.
|
Update synchronization parameters for a periodic sync that was already established.
When a sync is established by scanning (see Periodic Advertising Sync Scanner) or by receiving Periodic Advertising Synchronization Transfer (see PAST Receiver), the sync gets the skip and timeout parameters that were configured in the corresponding class. The application can use this command sl_bt_sync_update_sync_parameters to update the values of a sync that has been established. The application can for example update the values to better match the actual interval of the periodic advertising train, or to increase the skip value to minimize wakeups when power saving is prioritized over receiving every periodic advertisement.
Returns
SL_STATUS_OK if successful. Error code otherwise.
sl_bt_sync_close#
sl_status_t sl_bt_sync_close (uint16_t sync)
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint16_t | [in] | sync | Periodic advertising synchronization handle |
Close a periodic advertising synchronization or cancel an ongoing attempt of establishing a synchronization.
Returns
SL_STATUS_OK if successful. Error code otherwise.
Events
sl_bt_evt_sync_closed - Triggered after a periodic advertising synchronization has been closed or canceled.