Connection Analyzer Configuration flags#
Defines the configuration flags in connection analyzer.
Macros#
#define
Macro Definition Documentation#
SL_BT_CONNECTION_ANALYZER_RELATIVE_TIME#
#define SL_BT_CONNECTION_ANALYZER_RELATIVE_TIMEValue:
0x1
Indicates a given time value, e.g., start_time_us
in sl_bt_connection_analyzer_start, is a value relative to the current time.
Definition at line
15113
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h