sl_bt_evt_connection_analyzer_completed#

Triggered when the operation of analyzing a connection is completed.

Modules#

sl_bt_evt_connection_analyzer_completed_s

Macros#

#define

Identifier of the completed event.

Typedef Documentation#

sl_bt_evt_connection_analyzer_completed_t#

typedef struct sl_bt_evt_connection_analyzer_completed_s sl_bt_evt_connection_analyzer_completed_t

Definition at line 15162 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_connection_analyzer_completed_id#

#define sl_bt_evt_connection_analyzer_completed_id
Value:
0x014800a0

Identifier of the completed event.


Definition at line 15151 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h