Data structure of the completed event.

Public Attributes#

uint8_t
uint16_t

Public Attribute Documentation#

analyzer#

uint8_t sl_bt_evt_connection_analyzer_completed_s::analyzer

The handle of the connection analyzer


Definition at line 15158 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

reason#

uint16_t sl_bt_evt_connection_analyzer_completed_s::reason

The reason of stopping the operation


Definition at line 15159 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h