sl_bt_evt_connection_data_length#
Reports a change to the maximum payload length or maximum TX time in either direction of a connection.
Modules#
sl_bt_evt_connection_data_length_s
Typedefs#
Macros#
#define
sl_bt_evt_connection_data_length_id 0x090600a0
Identifier of the data_length event.
Typedef Documentation#
sl_bt_evt_connection_data_length_t#
typedef struct sl_bt_evt_connection_data_length_s sl_bt_evt_connection_data_length_t
Definition at line
6923
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_connection_data_length_id#
#define sl_bt_evt_connection_data_length_idValue:
0x090600a0
Identifier of the data_length event.
Definition at line
6905
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h