sl_bt_evt_connection_remote_used_features#
List of link layer features supported by the remote device.
Modules#
sl_bt_evt_connection_remote_used_features_s
Typedefs#
Macros#
#define
sl_bt_evt_connection_remote_used_features_id 0x080600a0
Identifier of the remote_used_features event.
Typedef Documentation#
sl_bt_evt_connection_remote_used_features_t#
typedef struct sl_bt_evt_connection_remote_used_features_s sl_bt_evt_connection_remote_used_features_t
Definition at line
6893
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_connection_remote_used_features_id#
#define sl_bt_evt_connection_remote_used_features_idValue:
0x080600a0
Identifier of the remote_used_features event.
Definition at line
6876
of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h