sl_bt_evt_system_error#

Indicates that an error has occurred.

See error codes table for more information.

Modules#

sl_bt_evt_system_error_s

Macros#

#define

Identifier of the error event.

Typedef Documentation#

sl_bt_evt_system_error_t#

typedef struct sl_bt_evt_system_error_s sl_bt_evt_system_error_t

Definition at line 833 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_system_error_id#

#define sl_bt_evt_system_error_id
Value:
0x060100a0

Identifier of the error event.


Definition at line 822 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h