sl_bt_evt_system_external_signal#

Indicates that the external signals have been received.

External signals are generated from the native application.

Modules#

sl_bt_evt_system_external_signal_s

Macros#

#define

Identifier of the external_signal event.

Typedef Documentation#

sl_bt_evt_system_external_signal_t#

typedef struct sl_bt_evt_system_external_signal_s sl_bt_evt_system_external_signal_t

Definition at line 943 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_system_external_signal_id#

#define sl_bt_evt_system_external_signal_id
Value:
0x030100a0

Identifier of the external_signal event.


Definition at line 932 of file /mnt/raid/workspaces/ws.iUTchugV0/overlay/gsdk/protocol/bluetooth/build_release/bt_api/sw/bgapi/inc/sl_bt_api.h