Extended Advertiser#

Extended Advertiser.

The commands and events in this class are related to extended advertising functionalities in GAP peripheral and broadcaster roles.

Modules#

Extended Advertising Configuration Flags

Enumerations#

enum
sl_bt_extended_advertiser_non_connectable = 0x0
sl_bt_extended_advertiser_scannable = 0x3
sl_bt_extended_advertiser_connectable = 0x4
}

These values define the available connection modes in extended advertising.

Functions#

sl_status_t
sl_bt_extended_advertiser_set_phy(uint8_t advertising_set, uint8_t primary_phy, uint8_t secondary_phy)
sl_status_t
sl_bt_extended_advertiser_set_data(uint8_t advertising_set, size_t data_len, const uint8_t *data)
sl_status_t
sl_status_t
sl_bt_extended_advertiser_generate_data(uint8_t advertising_set, uint8_t discover)
sl_status_t
sl_bt_extended_advertiser_start(uint8_t advertising_set, uint8_t connect, uint32_t flags)
sl_status_t
sl_bt_extended_advertiser_start_directed(uint8_t advertising_set, uint8_t connect, uint32_t flags, bd_addr peer_addr, uint8_t peer_addr_type)

Enumeration Documentation#

sl_bt_extended_advertiser_connection_mode_t#

sl_bt_extended_advertiser_connection_mode_t

These values define the available connection modes in extended advertising.

Enumerator
sl_bt_extended_advertiser_non_connectable

(0x0) Non-connectable and non-scannable extended advertising

sl_bt_extended_advertiser_scannable

(0x3) Scannable extended advertising

sl_bt_extended_advertiser_connectable

(0x4) Connectable extended advertising


Definition at line 2644 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

Function Documentation#

sl_bt_extended_advertiser_set_phy#

sl_status_t sl_bt_extended_advertiser_set_phy (uint8_t advertising_set, uint8_t primary_phy, uint8_t secondary_phy)
Parameters
[in]advertising_set

Advertising set handle

[in]primary_phy

Enum sl_bt_gap_phy_t. The PHY on which the advertising packets are transmitted on the primary advertising channel. Values:

  • sl_bt_gap_phy_1m (0x1): 1M PHY

  • sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8)

  • Default : sl_bt_gap_phy_1m

[in]secondary_phy

Enum sl_bt_gap_phy_t. The PHY on which the advertising packets are transmitted on the secondary advertising channel. Values:

  • sl_bt_gap_phy_1m (0x1): 1M PHY

  • sl_bt_gap_phy_2m (0x2): 2M PHY

  • sl_bt_gap_phy_coded (0x4): Coded PHY, 125k (S=8)

  • Default : sl_bt_gap_phy_1m

Set the primary and secondary advertising PHYs used for extended and periodic advertising on an advertising set. This setting will take effect next time extended or periodic advertising is enabled. When advertising on the LE Coded PHY, coding scheme S=8 is used. The SL_STATUS_INVALID_PARAMETER error is returned if a PHY value is invalid or the device does not support a given PHY.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 2702 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_extended_advertiser_set_data#

sl_status_t sl_bt_extended_advertiser_set_data (uint8_t advertising_set, size_t data_len, const uint8_t * data)
Parameters
[in]advertising_set

Advertising set handle

[in]data_len

Length of data in data

[in]data

Data to be set

Set user-defined data for extended advertising. This overwrites the existing advertising data packet and scan response packet on this advertising set regardless of whether the data was set for the legacy or extended advertising. Maximum 191 bytes of data can be set for connectable extended advertising. Maximum 253 bytes of data can be set for non-connectable extended advertising. For setting longer advertising data, use command sl_bt_extended_advertiser_set_long_data.

If advertising mode is currently enabled, the new advertising data will be used immediately. Advertising mode can be enabled using command sl_bt_extended_advertiser_start.

The invalid parameter error is returned if the data is too long to fit into a single advertisement.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 2730 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_extended_advertiser_set_long_data#

sl_status_t sl_bt_extended_advertiser_set_long_data (uint8_t advertising_set)
Parameters
[in]advertising_set

Advertising set handle

Set long user-defined data for extended advertising. This overwrites the existing advertising data packet and scan response packet on this advertising set regardless of whether the data was set for the legacy or extended advertising.

Prior to calling this command, add data to the buffer with one or multiple calls to sl_bt_system_data_buffer_write. When this command is called, the data in the system data buffer is extracted as the advertising data. The buffer will be emptied after this command regardless of the completion status.

Maximum 191 bytes of data can be set for connectable extended advertising. Maximum 1650 bytes of data can be set for non-connectable extended advertising. Advertising parameters may limit the amount of data that can be sent in a single advertisement. See sl_bt_extended_advertiser_set_data for more details.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 2758 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_extended_advertiser_generate_data#

sl_status_t sl_bt_extended_advertiser_generate_data (uint8_t advertising_set, uint8_t discover)
Parameters
[in]advertising_set

Advertising set handle

[in]discover

Enum sl_bt_advertiser_discovery_mode_t. The discovery mode for the Flags data field in the packet. Values:

  • sl_bt_advertiser_non_discoverable (0x0): Not discoverable

  • sl_bt_advertiser_limited_discoverable (0x1): Discoverable by both limited and general discovery procedures

  • sl_bt_advertiser_general_discoverable (0x2): Discoverable by the general discovery procedure

Ask the stack to generate the extended advertising data on an advertising set. Alternatively, user-defined advertising data can be set using the sl_bt_extended_advertiser_set_data command.

This overwrites the existing advertising data packet and scan response packet on this advertising set regardless of whether the data was set for the legacy or extended advertising.

If advertising mode is currently enabled, the new advertising data will be used immediately. To enable advertising mode, use command sl_bt_extended_advertiser_start.

See sl_bt_legacy_advertiser_generate_data for the advertising data generation logic.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 2789 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_extended_advertiser_start#

sl_status_t sl_bt_extended_advertiser_start (uint8_t advertising_set, uint8_t connect, uint32_t flags)
Parameters
[in]advertising_set

Advertising set handle

[in]connect

Enum sl_bt_extended_advertiser_connection_mode_t. Connection mode. Values:

  • sl_bt_extended_advertiser_non_connectable (0x0): Non-connectable and non-scannable extended advertising

  • sl_bt_extended_advertiser_scannable (0x3): Scannable extended advertising

  • sl_bt_extended_advertiser_connectable (0x4): Connectable extended advertising

[in]flags

Additional extended advertising options. Value: 0 or bitmask of Extended Advertising Configuration Flags

Start undirected extended advertising on an advertising set with the specified connection mode. Use sl_bt_advertiser_stop to stop the advertising.

Use the sl_bt_extended_advertiser_set_data or sl_bt_extended_advertiser_generate_data command to set the advertising data before calling this command. Advertising data is added into the scan response packet if the connection mode is scannable. Otherwise, data is in the advertising data packet.

The number of concurrent connectable advertisings is limited by the connection number configuration. See sl_bt_legacy_advertiser_start for more details.

This command fails with the invalid parameter error if the advertising uses a non-resolvable random address but the connection mode is sl_bt_extended_advertiser_connectable.

This command returns the error SL_STATUS_BT_CONTROLLER_COMMAND_DISALLOWED when the connection mode is sl_bt_extended_advertiser_scannable but no scan response data is provided.

Event sl_bt_evt_connection_opened will be received when a remote device opens a connection to the advertiser on this advertising set. As a result, the advertising stops.

Event sl_bt_evt_advertiser_timeout will be received when the number of advertising events set by sl_bt_advertiser_set_timing command is done and the advertising has stopped.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 2846 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_extended_advertiser_start_directed#

sl_status_t sl_bt_extended_advertiser_start_directed (uint8_t advertising_set, uint8_t connect, uint32_t flags, bd_addr peer_addr, uint8_t peer_addr_type)
Parameters
[in]advertising_set

Advertising set handle

[in]connect

Enum sl_bt_extended_advertiser_connection_mode_t. Connection mode. Values:

  • sl_bt_extended_advertiser_non_connectable (0x0): Non-connectable and non-scannable extended advertising

  • sl_bt_extended_advertiser_scannable (0x3): Scannable extended advertising

  • sl_bt_extended_advertiser_connectable (0x4): Connectable extended advertising

[in]flags

Additional extended advertising options. Value: 0 or bitmask of Extended Advertising Configuration Flags

[in]peer_addr

Address of the peer target device the advertising is directed to

[in]peer_addr_type

Enum sl_bt_gap_address_type_t.

Peer target device address type.

If the application does not include the bluetooth_feature_use_accurate_api_address_types component, peer_addr_type uses the following values:

  • 0: Public address

  • 1: Random address

If the application includes the bluetooth_feature_use_accurate_api_address_types component, peer_addr_type uses enum sl_bt_gap_address_type_t values:

  • sl_bt_gap_public_address (0x0): Public device address

  • sl_bt_gap_static_address (0x1): Static device address

  • sl_bt_gap_random_resolvable_address (0x2): Resolvable private random address

  • sl_bt_gap_random_nonresolvable_address (0x3): Non-resolvable private random address

  • sl_bt_gap_public_address_resolved_from_rpa (0x4): Public identity address resolved from a resolvable private address (RPA)

  • sl_bt_gap_static_address_resolved_from_rpa (0x5): Static identity address resolved from a resolvable private address (RPA)

Start directed extended advertising on an advertising set with the specified peer target device and connection mode. Use sl_bt_advertiser_stop to stop the advertising.

The number of concurrent connectable advertisings is limited by the connection number configuration. See sl_bt_legacy_advertiser_start for more details.

This command fails with the invalid parameter error if the advertising uses a non-resolvable random address but the connection mode is sl_bt_extended_advertiser_connectable.

Event sl_bt_evt_connection_opened will be received when the target device opens a connection to the advertiser on this advertising set. As a result, the advertising stops.

Event sl_bt_evt_advertiser_timeout will be received when the advertising stops and no Bluetooth connection is opened to it.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 2920 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_cmd_extended_advertiser_set_phy_id#

#define sl_bt_cmd_extended_advertiser_set_phy_id
Value:
0x00570020

Definition at line 2627 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_extended_advertiser_set_data_id#

#define sl_bt_cmd_extended_advertiser_set_data_id
Value:
0x01570020

Definition at line 2628 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_extended_advertiser_set_long_data_id#

#define sl_bt_cmd_extended_advertiser_set_long_data_id
Value:
0x02570020

Definition at line 2629 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_extended_advertiser_generate_data_id#

#define sl_bt_cmd_extended_advertiser_generate_data_id
Value:
0x03570020

Definition at line 2630 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_extended_advertiser_start_id#

#define sl_bt_cmd_extended_advertiser_start_id
Value:
0x04570020

Definition at line 2631 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_extended_advertiser_start_directed_id#

#define sl_bt_cmd_extended_advertiser_start_directed_id
Value:
0x05570020

Definition at line 2632 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_extended_advertiser_set_phy_id#

#define sl_bt_rsp_extended_advertiser_set_phy_id
Value:
0x00570020

Definition at line 2633 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_extended_advertiser_set_data_id#

#define sl_bt_rsp_extended_advertiser_set_data_id
Value:
0x01570020

Definition at line 2634 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_extended_advertiser_set_long_data_id#

#define sl_bt_rsp_extended_advertiser_set_long_data_id
Value:
0x02570020

Definition at line 2635 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_extended_advertiser_generate_data_id#

#define sl_bt_rsp_extended_advertiser_generate_data_id
Value:
0x03570020

Definition at line 2636 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_extended_advertiser_start_id#

#define sl_bt_rsp_extended_advertiser_start_id
Value:
0x04570020

Definition at line 2637 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_extended_advertiser_start_directed_id#

#define sl_bt_rsp_extended_advertiser_start_directed_id
Value:
0x05570020

Definition at line 2638 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h