GATT Server#

GATT Server.

These commands and events are used for accessing to the local GATT server and database.

Modules#

sl_bt_evt_gatt_server_attribute_value

sl_bt_evt_gatt_server_user_read_request

sl_bt_evt_gatt_server_user_write_request

sl_bt_evt_gatt_server_characteristic_status

sl_bt_evt_gatt_server_execute_write_completed

sl_bt_evt_gatt_server_indication_timeout

sl_bt_evt_gatt_server_notification_tx_completed

Enumerations#

enum
sl_bt_gatt_server_disable = 0x0
sl_bt_gatt_server_notification = 0x1
sl_bt_gatt_server_indication = 0x2
sl_bt_gatt_server_notification_and_indication = 0x3
}

These values define whether the server is to sent notifications or indications to a remote GATT server.

enum
sl_bt_gatt_server_client_config = 0x1
sl_bt_gatt_server_confirmation = 0x2
}

These values describe whether the characteristic client configuration was changed or whether a characteristic confirmation was received.

Functions#

sl_status_t
sl_bt_gatt_server_set_max_mtu(uint16_t max_mtu, uint16_t *max_mtu_out)
sl_status_t
sl_bt_gatt_server_get_mtu(uint8_t connection, uint16_t *mtu)
sl_status_t
sl_bt_gatt_server_find_attribute(uint16_t start, size_t type_len, const uint8_t *type, uint16_t *attribute)
sl_status_t
sl_bt_gatt_server_read_attribute_value(uint16_t attribute, uint16_t offset, size_t max_value_size, size_t *value_len, uint8_t *value)
sl_status_t
sl_bt_gatt_server_read_attribute_type(uint16_t attribute, size_t max_type_size, size_t *type_len, uint8_t *type)
sl_status_t
sl_bt_gatt_server_write_attribute_value(uint16_t attribute, uint16_t offset, size_t value_len, const uint8_t *value)
sl_status_t
sl_bt_gatt_server_send_user_read_response(uint8_t connection, uint16_t characteristic, uint8_t att_errorcode, size_t value_len, const uint8_t *value, uint16_t *sent_len)
sl_status_t
sl_bt_gatt_server_send_user_write_response(uint8_t connection, uint16_t characteristic, uint8_t att_errorcode)
sl_status_t
sl_bt_gatt_server_send_notification(uint8_t connection, uint16_t characteristic, size_t value_len, const uint8_t *value)
sl_status_t
sl_bt_gatt_server_send_indication(uint8_t connection, uint16_t characteristic, size_t value_len, const uint8_t *value)
sl_status_t
sl_bt_gatt_server_notify_all(uint16_t characteristic, size_t value_len, const uint8_t *value)
sl_status_t
sl_bt_gatt_server_read_client_configuration(uint8_t connection, uint16_t characteristic, uint16_t *client_config_flags)
sl_status_t
sl_bt_gatt_server_send_user_prepare_write_response(uint8_t connection, uint16_t characteristic, uint8_t att_errorcode, uint16_t offset, size_t value_len, const uint8_t *value)
sl_status_t
sl_bt_gatt_server_set_capabilities(uint32_t caps, uint32_t reserved)
sl_status_t
sl_status_t
sl_status_t
sl_bt_gatt_server_read_client_supported_features(uint8_t connection, uint8_t *client_features)

Macros#

Enumeration Documentation#

sl_bt_gatt_server_client_configuration_t#

sl_bt_gatt_server_client_configuration_t

These values define whether the server is to sent notifications or indications to a remote GATT server.

Enumerator
sl_bt_gatt_server_disable

(0x0) Disable notifications and indications.

sl_bt_gatt_server_notification

(0x1) The characteristic value shall be notified.

sl_bt_gatt_server_indication

(0x2) The characteristic value shall be indicated.

sl_bt_gatt_server_notification_and_indication

(0x3) The characteristic value notification and indication are enabled, application decides which one to send.


Definition at line 8603 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_characteristic_status_flag_t#

sl_bt_gatt_server_characteristic_status_flag_t

These values describe whether the characteristic client configuration was changed or whether a characteristic confirmation was received.

Enumerator
sl_bt_gatt_server_client_config

(0x1) Characteristic client configuration has been changed.

sl_bt_gatt_server_confirmation

(0x2) Characteristic confirmation has been received.


Definition at line 8627 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

Function Documentation#

sl_bt_gatt_server_set_max_mtu#

sl_status_t sl_bt_gatt_server_set_max_mtu (uint16_t max_mtu, uint16_t * max_mtu_out)
Parameters
[in]max_mtu

Maximum size of Message Transfer Units (MTU) allowed

  • Range: 23 to 250

  • Default : 247

[out]max_mtu_out

The maximum ATT_MTU selected by the system if this command succeeded

Set the maximum size of ATT Message Transfer Units (MTU). The functionality is the same as sl_bt_gatt_set_max_mtu and this setting applies to both GATT client and server. If the given value is too large according to the maximum BGAPI payload size, the system will select the maximum possible value as the maximum ATT_MTU. If the maximum ATT_MTU is larger than 23, the GATT client in the stack will automatically send an MTU exchange request after a Bluetooth connection was established.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 8902 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_get_mtu#

sl_status_t sl_bt_gatt_server_get_mtu (uint8_t connection, uint16_t * mtu)
Parameters
[in]connection

Connection handle

[out]mtu

The maximum ATT_MTU used by the connection

Get the size of ATT Message Transfer Units (MTU) for a connection.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 8915 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_find_attribute#

sl_status_t sl_bt_gatt_server_find_attribute (uint16_t start, size_t type_len, const uint8_t * type, uint16_t * attribute)
Parameters
[in]start

Search start handle

[in]type_len

Length of data in type

[in]type

The attribute type UUID

[out]attribute

Attribute handle

Find attributes of a certain type from a local GATT database. The type is usually given as a 16-bit or 128-bit UUID in little endian format.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 8930 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_read_attribute_value#

sl_status_t sl_bt_gatt_server_read_attribute_value (uint16_t attribute, uint16_t offset, size_t max_value_size, size_t * value_len, uint8_t * value)
Parameters
[in]attribute

Attribute handle

[in]offset

Value offset

[in]max_value_size

Size of output buffer passed in value

[out]value_len

On return, set to the length of output data written to value

[out]value

The attribute value

Read the value of an attribute from a local GATT database. Only (maximum BGAPI payload size - 3) amount of data can be read at once. The application can continue reading with increased offset value if it receives (maximum BGAPI payload size - 3) number of bytes.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 8952 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_read_attribute_type#

sl_status_t sl_bt_gatt_server_read_attribute_type (uint16_t attribute, size_t max_type_size, size_t * type_len, uint8_t * type)
Parameters
[in]attribute

Attribute handle

[in]max_type_size

Size of output buffer passed in type

[out]type_len

On return, set to the length of output data written to type

[out]type

The attribute type UUID

Read the type of an attribute from a local GATT database. The type is a UUID, usually 16 or 128 bits long in little endian format.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 8972 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_write_attribute_value#

sl_status_t sl_bt_gatt_server_write_attribute_value (uint16_t attribute, uint16_t offset, size_t value_len, const uint8_t * value)
Parameters
[in]attribute

Attribute handle

[in]offset

Value offset

[in]value_len

Length of data in value

[in]value

Value

Write the value of an attribute in the local GATT database. Writing the value of a characteristic of the local GATT database will not trigger notifications or indications to the remote GATT client if the characteristic has a property to indicate or notify and the client has enabled notification or indication. Notifications and indications are sent to the remote GATT client using sl_bt_gatt_server_send_notification or sl_bt_gatt_server_send_indication commands.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 8995 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_send_user_read_response#

sl_status_t sl_bt_gatt_server_send_user_read_response (uint8_t connection, uint16_t characteristic, uint8_t att_errorcode, size_t value_len, const uint8_t * value, uint16_t * sent_len)
Parameters
[in]connection

Connection handle

[in]characteristic

GATT characteristic handle received in the sl_bt_evt_gatt_server_user_read_request event.

[in]att_errorcode

Attribute protocol error code

  • 0: No error

  • Non-zero: See Bluetooth specification, Host volume, Attribute Protocol, Error Codes table.

[in]value_len

Length of data in value

[in]value

Characteristic value to send to the GATT client. Ignored if att_errorcode is not 0.

[out]sent_len

The length of data sent to the remote GATT client

Send a response to a sl_bt_evt_gatt_server_user_read_request event. The response needs to be sent within 30 seconds, otherwise no more GATT transactions are allowed by the remote side. If attr_errorcode is set to 0, the characteristic value is sent to the remote GATT client in the standard way. Other attr_errorcode values will cause the local GATT server to send an attribute protocol error response instead of the actual data. Maximum number of bytes this command can send depends on the value of parameter att_opcode in sl_bt_evt_gatt_server_user_read_request event:

If the data length in value exceeds the limit, the first maximum number of bytes will be sent and rest data is ignored. The actual number of bytes that was sent is retruned in the response of this command.

The client will continue reading by sending a new read blob request with an increased offset value if it receives the maximum amount of attribute data the read respond packet can contain.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 9037 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_send_user_write_response#

sl_status_t sl_bt_gatt_server_send_user_write_response (uint8_t connection, uint16_t characteristic, uint8_t att_errorcode)
Parameters
[in]connection

Connection handle

[in]characteristic

GATT characteristic handle received in the sl_bt_evt_gatt_server_user_write_request event

[in]att_errorcode

Attribute protocol error code

  • 0: No error

  • Non-zero: See Bluetooth specification, Host volume, Attribute Protocol, Error Codes table.

Send a response to a sl_bt_evt_gatt_server_user_write_request event when parameter att_opcode in the event is sl_bt_gatt_write_request or sl_bt_gatt_execute_write_request (see sl_bt_gatt_att_opcode_t). The response needs to be sent within 30 seconds, otherwise no more GATT transactions are allowed by the remote side. When responding to sl_bt_gatt_execute_write_request, the value of parameter characteristic is ignored. If attr_errorcode is set to 0, the ATT protocol's write response is sent to indicate to the remote GATT client that the write operation was processed successfully. Other values will cause the local GATT server to send an ATT protocol error response.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 9068 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_send_notification#

sl_status_t sl_bt_gatt_server_send_notification (uint8_t connection, uint16_t characteristic, size_t value_len, const uint8_t * value)
Parameters
[in]connection

A handle of the connection over which the notification is sent.

[in]characteristic

Characteristic handle

[in]value_len

Length of data in value

[in]value

Value to be notified

Send a notification to a remote GATT client. At most, ATT_MTU - 3 number of bytes can be sent in a notification. An error SL_STATUS_COMMAND_TOO_LONG is returned if the value length exceeds ATT_MTU - 3.

A notification is sent only if the client has enabled it by setting the corresponding flag to the Client Characteristic Configuration descriptor. The error SL_STATUS_INVALID_PARAMETER is returned if the characteristic does not have the notification property. The error SL_STATUS_INVALID_STATE is returned if the client has not enabled the notification.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 9093 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_send_indication#

sl_status_t sl_bt_gatt_server_send_indication (uint8_t connection, uint16_t characteristic, size_t value_len, const uint8_t * value)
Parameters
[in]connection

A handle of the connection over which the indication is sent.

[in]characteristic

Characteristic handle

[in]value_len

Length of data in value

[in]value

Value to be indicated

Send an indication to a remote GATT client. At most, ATT_MTU - 3 number of bytes can be sent in an indication. An error SL_STATUS_COMMAND_TOO_LONG is returned if the value length exceeds ATT_MTU - 3.

An indication is sent only if the client has enabled it by setting the corresponding flag to the Client Characteristic Configuration descriptor. The error SL_STATUS_INVALID_PARAMETER is returned if the characteristic does not have the indication property. The error SL_STATUS_INVALID_STATE is returned if the client has not enabled the indication.

A new indication to a GATT client can't be sent until an outstanding indication procedure with the same client has completed. The procedure is completed when a confirmation from the client is received. The confirmation is indicated by sl_bt_evt_gatt_server_characteristic_status.

The error SL_STATUS_IN_PROGRESS is returned if an indication procedure with the same client is outstanding. Always wait for confirmation for previous indication before sending a new indication.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.

Events


Definition at line 9136 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_notify_all#

sl_status_t sl_bt_gatt_server_notify_all (uint16_t characteristic, size_t value_len, const uint8_t * value)
Parameters
[in]characteristic

Characteristic handle

[in]value_len

Length of data in value

[in]value

Value to be notified or indicated

Send notifications or indications to all connected remote GATT clients. At most, ATT_MTU - 3 number of bytes can be sent in a notification or indication. If the value length exceeds the limit on a connection, the first ATT_MTU - 3 bytes will be sent and rest of data is ignored.

A notification or indication is sent only if the client has enabled it by setting the corresponding flag to the Client Characteristic Configuration descriptor. If the Client Characteristic Configuration descriptor supports both notifications and indications, the stack will always send a notification even when the client has enabled both.

A new indication to a GATT client can't be sent until an outstanding indication procedure with the same client has completed, and the operation will continue for the next client. The procedure is completed when a confirmation from the client is received. The confirmation is indicated by sl_bt_evt_gatt_server_characteristic_status.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 9167 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_read_client_configuration#

sl_status_t sl_bt_gatt_server_read_client_configuration (uint8_t connection, uint16_t characteristic, uint16_t * client_config_flags)
Parameters
[in]connection

A handle of the connection to a remote client.

[in]characteristic

Characteristic handle

[out]client_config_flags

Enum sl_bt_gatt_server_client_configuration_t. Client characteristic configuration of a remote client.

Read client characteristic configuration of a remote GATT client.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 9184 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_send_user_prepare_write_response#

sl_status_t sl_bt_gatt_server_send_user_prepare_write_response (uint8_t connection, uint16_t characteristic, uint8_t att_errorcode, uint16_t offset, size_t value_len, const uint8_t * value)
Parameters
[in]connection

Connection handle

[in]characteristic

GATT characteristic handle. This value is normally received from the gatt_characteristic event.

[in]att_errorcode

Attribute protocol error code

  • 0: No error

  • Non-zero: See Bluetooth specification, Host volume, Attribute Protocol, Error Codes table.

[in]offset

Value offset

[in]value_len

Length of data in value

[in]value

Value

Send a response to a sl_bt_evt_gatt_server_user_write_request event when parameter att_opcode in the event is sl_bt_gatt_prepare_write_request (see sl_bt_gatt_att_opcode_t). The response needs to be sent within 30 seconds, otherwise no more GATT transactions are allowed by the remote side. If att_errorcode is set to 0, the ATT protocol's prepare write response is sent to indicate to the remote GATT client that the write operation was processed successfully. Other values will cause the local GATT server to send an ATT protocol error response. The application should set values of parameters offset and value to identical values from the sl_bt_evt_gatt_server_user_write_request event. The values will be verified on the client side in case the request is a reliable write (by Bluetooth Core Specification Volume 3, Part G, 4.9.5).

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 9217 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_set_capabilities#

sl_status_t sl_bt_gatt_server_set_capabilities (uint32_t caps, uint32_t reserved)
Parameters
[in]caps

Bit flags of capabilities to reset. Value 0 sets the default database capabilities.

[in]reserved

Use the value 0 on this reserved field. Do not use none-zero values because they are reserved for future use.

Reset capabilities that should be enabled by the GATT database. A service is visible to remote GATT clients if at least one of its capabilities is enabled. The same applies to a characteristic and its attributes. Capability identifiers and their corresponding bit flag values are in the auto-generated database header file. See UG118: Blue Gecko Bluetooth Profile Toolkit Developer's Guide for how to declare capabilities in the GATT database.

Changing the capabilities of a database effectively causes a database change (attributes being added or removed) from a remote GATT client point of view. If the database has a Generic Attribute service and Service Changed characteristic, the stack will monitor the local database change status and manage service changed indications for a GATT client that has enabled the indication configuration of the Service Changed characteristic.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 9248 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_enable_capabilities#

sl_status_t sl_bt_gatt_server_enable_capabilities (uint32_t caps)
Parameters
[in]caps

Capabilities to enable

Enable additional capabilities in the local GATT database. Already enabled capabilities keep unchanged after this command. See sl_bt_gatt_server_set_capabilities for more information.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 9262 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_disable_capabilities#

sl_status_t sl_bt_gatt_server_disable_capabilities (uint32_t caps)
Parameters
[in]caps

Capabilities to disable

Disable the given capabilities in the local GATT database. See sl_bt_gatt_server_set_capabilities for more information.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 9274 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_get_enabled_capabilities#

sl_status_t sl_bt_gatt_server_get_enabled_capabilities (uint32_t * caps)
Parameters
[out]caps

Enabled capabilities

Get capabilities currently enabled in the local GATT database.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 9285 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_gatt_server_read_client_supported_features#

sl_status_t sl_bt_gatt_server_read_client_supported_features (uint8_t connection, uint8_t * client_features)
Parameters
[in]connection

A handle of the connection to a remote client.

[out]client_features

Bit field describing client supported features of a remote client. See Bluetooth specification Vol 3, Part G, 7.2 for the values.

Read client supported features of a remote GATT client.

Returns

  • SL_STATUS_OK if successful. Error code otherwise.


Definition at line 9299 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_cmd_gatt_server_set_max_mtu_id#

#define sl_bt_cmd_gatt_server_set_max_mtu_id
Value:
0x0a0a0020

Definition at line 8562 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_get_mtu_id#

#define sl_bt_cmd_gatt_server_get_mtu_id
Value:
0x0b0a0020

Definition at line 8563 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_find_attribute_id#

#define sl_bt_cmd_gatt_server_find_attribute_id
Value:
0x060a0020

Definition at line 8564 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_read_attribute_value_id#

#define sl_bt_cmd_gatt_server_read_attribute_value_id
Value:
0x000a0020

Definition at line 8565 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_read_attribute_type_id#

#define sl_bt_cmd_gatt_server_read_attribute_type_id
Value:
0x010a0020

Definition at line 8566 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_write_attribute_value_id#

#define sl_bt_cmd_gatt_server_write_attribute_value_id
Value:
0x020a0020

Definition at line 8567 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_send_user_read_response_id#

#define sl_bt_cmd_gatt_server_send_user_read_response_id
Value:
0x030a0020

Definition at line 8568 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_send_user_write_response_id#

#define sl_bt_cmd_gatt_server_send_user_write_response_id
Value:
0x040a0020

Definition at line 8569 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_send_notification_id#

#define sl_bt_cmd_gatt_server_send_notification_id
Value:
0x0f0a0020

Definition at line 8570 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_send_indication_id#

#define sl_bt_cmd_gatt_server_send_indication_id
Value:
0x100a0020

Definition at line 8571 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_notify_all_id#

#define sl_bt_cmd_gatt_server_notify_all_id
Value:
0x110a0020

Definition at line 8572 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_read_client_configuration_id#

#define sl_bt_cmd_gatt_server_read_client_configuration_id
Value:
0x120a0020

Definition at line 8573 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_send_user_prepare_write_response_id#

#define sl_bt_cmd_gatt_server_send_user_prepare_write_response_id
Value:
0x140a0020

Definition at line 8574 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_set_capabilities_id#

#define sl_bt_cmd_gatt_server_set_capabilities_id
Value:
0x080a0020

Definition at line 8575 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_enable_capabilities_id#

#define sl_bt_cmd_gatt_server_enable_capabilities_id
Value:
0x0c0a0020

Definition at line 8576 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_disable_capabilities_id#

#define sl_bt_cmd_gatt_server_disable_capabilities_id
Value:
0x0d0a0020

Definition at line 8577 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_get_enabled_capabilities_id#

#define sl_bt_cmd_gatt_server_get_enabled_capabilities_id
Value:
0x0e0a0020

Definition at line 8578 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_cmd_gatt_server_read_client_supported_features_id#

#define sl_bt_cmd_gatt_server_read_client_supported_features_id
Value:
0x150a0020

Definition at line 8579 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_set_max_mtu_id#

#define sl_bt_rsp_gatt_server_set_max_mtu_id
Value:
0x0a0a0020

Definition at line 8580 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_get_mtu_id#

#define sl_bt_rsp_gatt_server_get_mtu_id
Value:
0x0b0a0020

Definition at line 8581 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_find_attribute_id#

#define sl_bt_rsp_gatt_server_find_attribute_id
Value:
0x060a0020

Definition at line 8582 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_read_attribute_value_id#

#define sl_bt_rsp_gatt_server_read_attribute_value_id
Value:
0x000a0020

Definition at line 8583 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_read_attribute_type_id#

#define sl_bt_rsp_gatt_server_read_attribute_type_id
Value:
0x010a0020

Definition at line 8584 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_write_attribute_value_id#

#define sl_bt_rsp_gatt_server_write_attribute_value_id
Value:
0x020a0020

Definition at line 8585 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_send_user_read_response_id#

#define sl_bt_rsp_gatt_server_send_user_read_response_id
Value:
0x030a0020

Definition at line 8586 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_send_user_write_response_id#

#define sl_bt_rsp_gatt_server_send_user_write_response_id
Value:
0x040a0020

Definition at line 8587 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_send_notification_id#

#define sl_bt_rsp_gatt_server_send_notification_id
Value:
0x0f0a0020

Definition at line 8588 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_send_indication_id#

#define sl_bt_rsp_gatt_server_send_indication_id
Value:
0x100a0020

Definition at line 8589 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_notify_all_id#

#define sl_bt_rsp_gatt_server_notify_all_id
Value:
0x110a0020

Definition at line 8590 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_read_client_configuration_id#

#define sl_bt_rsp_gatt_server_read_client_configuration_id
Value:
0x120a0020

Definition at line 8591 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_send_user_prepare_write_response_id#

#define sl_bt_rsp_gatt_server_send_user_prepare_write_response_id
Value:
0x140a0020

Definition at line 8592 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_set_capabilities_id#

#define sl_bt_rsp_gatt_server_set_capabilities_id
Value:
0x080a0020

Definition at line 8593 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_enable_capabilities_id#

#define sl_bt_rsp_gatt_server_enable_capabilities_id
Value:
0x0c0a0020

Definition at line 8594 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_disable_capabilities_id#

#define sl_bt_rsp_gatt_server_disable_capabilities_id
Value:
0x0d0a0020

Definition at line 8595 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_get_enabled_capabilities_id#

#define sl_bt_rsp_gatt_server_get_enabled_capabilities_id
Value:
0x0e0a0020

Definition at line 8596 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

sl_bt_rsp_gatt_server_read_client_supported_features_id#

#define sl_bt_rsp_gatt_server_read_client_supported_features_id
Value:
0x150a0020

Definition at line 8597 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h