sl_bt_evt_gatt_server_execute_write_completed#

Indicates that the execute write command from a remote GATT client has completed with the given result.

Modules#

sl_bt_evt_gatt_server_execute_write_completed_s

Macros#

#define

Identifier of the execute_write_completed event.

Typedef Documentation#

sl_bt_evt_gatt_server_execute_write_completed_t#

typedef struct sl_bt_evt_gatt_server_execute_write_completed_s sl_bt_evt_gatt_server_execute_write_completed_t

Definition at line 8819 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_gatt_server_execute_write_completed_id#

#define sl_bt_evt_gatt_server_execute_write_completed_id
Value:
0x040a00a0

Identifier of the execute_write_completed event.


Definition at line 8808 of file /mnt/raid/workspaces/ws.wDIAeKYhQ/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h