Application OTA DFU#
Component that provides over-the-air (OTA) device firmware update (DFU) functionality in user application during runtime. No need to enter a specialized OTA state to update, and no AppLoader utility required. No code is required from user to enable this component.
Modules#
sl_bt_app_ota_dfu_btl_storage_info_t
sl_bt_app_ota_dfu_download_package_t
Enumerations#
enum
SL_BT_APP_OTA_DFU_UNINIT = 0
SL_BT_APP_OTA_DFU_INIT 
SL_BT_APP_OTA_DFU_READ_FLASH 
SL_BT_APP_OTA_DFU_ERASE 
SL_BT_APP_OTA_DFU_READY 
SL_BT_APP_OTA_DFU_DISCONNECT 
SL_BT_APP_OTA_DFU_DOWNLOAD_BEGIN 
SL_BT_APP_OTA_DFU_DOWNLOAD_END 
SL_BT_APP_OTA_DFU_VERIFY 
SL_BT_APP_OTA_DFU_FINALIZE 
SL_BT_APP_OTA_DFU_WAIT_FOR_REBOOT 
SL_BT_APP_OTA_DFU_ERROR 
}
enum
SL_BT_APP_OTA_DFU_NO_ERROR = 0
SL_BT_APP_OTA_DFU_ERR_GENERIC 
SL_BT_APP_OTA_DFU_ERR_UNEXPECTED_TRANSFER 
SL_BT_APP_OTA_DFU_ERR_UNEXPECTED_CLOSE 
SL_BT_APP_OTA_DFU_ERR_BOOTLOADER_API 
SL_BT_APP_OTA_DFU_ERR_STORAGE_FULL 
SL_BT_APP_OTA_DFU_ERR_INIT 
SL_BT_APP_OTA_DFU_ERR_ACQUIRE 
SL_BT_APP_OTA_DFU_ERR_RELEASE 
}
enum
SL_BT_APP_OTA_DFU_EVT_BTL_STORAGE_INFO_ID = 0u
SL_BT_APP_OTA_DFU_EVT_STATE_CHANGE_ID 
SL_BT_APP_OTA_DFU_EVT_DOWNLOAD_PACKET_ID 
SL_BT_APP_OTA_DFU_EVT_VERIFY_IMAGE_ID 
}
Typedefs#
typedef struct sl_bt_app_ota_dfu_msg_t
Functions#
sl_status_t
void
sl_bt_app_ota_dfu_reboot(void)
void
sl_bt_app_ota_dfu_on_status_event(sl_bt_app_ota_dfu_status_evt_t *evt)
Macros#
#define
SL_BT_APP_OTA_DFU_CONFIG_PRIORITY APP_RTA_PRIORITY_NORMAL
#define
SL_BT_APP_OTA_DFU_CONFIG_STACK 1024
#define
SL_BT_APP_OTA_DFU_CONFIG_WAIT 10
#define
SL_BT_APP_OTA_DFU_USED_SLOT 0u
#define
SL_BT_APP_OTA_DFU_READ_STORAGE_CONTEXT_SIZE 256u
#define
SL_BT_APP_OTA_DFU_EMPTY_FLASH_CONTENT 0xFFFFFFFFu
#define
SL_BT_APP_OTA_DFU_VERIFICATION_BLOCK_SIZE 128u
Enumeration Documentation#
sl_bt_app_ota_dfu_status_t#
sl_bt_app_ota_dfu_status_t
| Enumerator | |
|---|---|
| SL_BT_APP_OTA_DFU_UNINIT | |
| SL_BT_APP_OTA_DFU_INIT | |
| SL_BT_APP_OTA_DFU_READ_FLASH | |
| SL_BT_APP_OTA_DFU_ERASE | |
| SL_BT_APP_OTA_DFU_READY | |
| SL_BT_APP_OTA_DFU_DISCONNECT | |
| SL_BT_APP_OTA_DFU_DOWNLOAD_BEGIN | |
| SL_BT_APP_OTA_DFU_DOWNLOAD_END | |
| SL_BT_APP_OTA_DFU_VERIFY | |
| SL_BT_APP_OTA_DFU_FINALIZE | |
| SL_BT_APP_OTA_DFU_WAIT_FOR_REBOOT | |
| SL_BT_APP_OTA_DFU_ERROR | |
sl_bt_app_ota_dfu_error_t#
sl_bt_app_ota_dfu_error_t
| Enumerator | |
|---|---|
| SL_BT_APP_OTA_DFU_NO_ERROR | |
| SL_BT_APP_OTA_DFU_ERR_GENERIC | |
| SL_BT_APP_OTA_DFU_ERR_UNEXPECTED_TRANSFER | |
| SL_BT_APP_OTA_DFU_ERR_UNEXPECTED_CLOSE | |
| SL_BT_APP_OTA_DFU_ERR_BOOTLOADER_API | |
| SL_BT_APP_OTA_DFU_ERR_STORAGE_FULL | |
| SL_BT_APP_OTA_DFU_ERR_INIT | |
| SL_BT_APP_OTA_DFU_ERR_ACQUIRE | |
| SL_BT_APP_OTA_DFU_ERR_RELEASE | |
sl_bt_app_ota_dfu_event_id_t#
sl_bt_app_ota_dfu_event_id_t
| Enumerator | |
|---|---|
| SL_BT_APP_OTA_DFU_EVT_BTL_STORAGE_INFO_ID | |
| SL_BT_APP_OTA_DFU_EVT_STATE_CHANGE_ID | |
| SL_BT_APP_OTA_DFU_EVT_DOWNLOAD_PACKET_ID | |
| SL_BT_APP_OTA_DFU_EVT_VERIFY_IMAGE_ID | |
Typedef Documentation#
sl_bt_app_ota_dfu_status_evt_t#
typedef struct sl_bt_app_ota_dfu_msg_t sl_bt_app_ota_dfu_status_evt_t
Function Documentation#
sl_bt_app_ota_dfu_restart_progress#
sl_status_t sl_bt_app_ota_dfu_restart_progress (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Function to restart application OTA DFU progress without rebooting in case of any error.
Returns
status of the operation
sl_bt_app_ota_dfu_reboot#
void sl_bt_app_ota_dfu_reboot (void )
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| void | N/A | 
Function to reboot only when the application OTA DFU process is already in the SL_BT_APP_OTA_DFU_WAIT_FOR_REBOOT state.
sl_bt_app_ota_dfu_on_status_event#
void sl_bt_app_ota_dfu_on_status_event (sl_bt_app_ota_dfu_status_evt_t * evt)
Parameters
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| sl_bt_app_ota_dfu_status_evt_t * | [in] | evt | Actual app ota dfu event address.  | 
Function to indicate Application OTA DFU status and in case of error the error codes for assertion. Note
To be implemented in user code.