sl_bt_evt_connection_analyzer_report#

Triggered when packets transmitted on a connection are captured.

Modules#

sl_bt_evt_connection_analyzer_report_s

Macros#

#define

Identifier of the report event.

Typedef Documentation#

sl_bt_evt_connection_analyzer_report_t#

typedef struct sl_bt_evt_connection_analyzer_report_s sl_bt_evt_connection_analyzer_report_t

Definition at line 14572 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_connection_analyzer_report_id#

#define sl_bt_evt_connection_analyzer_report_id
Value:
0x004800a0

Identifier of the report event.


Definition at line 14556 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h