Data structure of the report event.

Public Attributes#

uint8_t

Public Attribute Documentation#

analyzer#

uint8_t sl_bt_evt_connection_analyzer_report_s::analyzer

The handle of the connection analyzer


Definition at line 14563 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

central_rssi#

int8_t sl_bt_evt_connection_analyzer_report_s::central_rssi

RSSI measurement of the packet transmitted by the Central device. Units: dBm.

  • Range: -127 to +20


Definition at line 14564 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

peripheral_rssi#

int8_t sl_bt_evt_connection_analyzer_report_s::peripheral_rssi

RSSI measurement of the packet transmitted by the Peripheral device. Units: dBm.

  • Range: -127 to +20


Definition at line 14567 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h