sl_bt_evt_cs_config_complete#

Indicates that a locally initiated CS configuration procedure has completed or the local controller has responded to an CS configuration request from the remote controller.

Modules#

sl_bt_evt_cs_config_complete_s

Macros#

#define
sl_bt_evt_cs_config_complete_id 0x015900a0

Identifier of the config_complete event.

Typedef Documentation#

sl_bt_evt_cs_config_complete_t#

typedef struct sl_bt_evt_cs_config_complete_s sl_bt_evt_cs_config_complete_t

Definition at line 11922 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h