sl_bt_evt_cs_read_remote_supported_capabilities_complete#

Report the remote controller's supported capabilities as a result of calling the sl_bt_cs_read_remote_supported_capabilities command previously.

Modules#

sl_bt_evt_cs_read_remote_supported_capabilities_complete_s

Macros#

#define

Identifier of the read_remote_supported_capabilities_complete event.

Typedef Documentation#

sl_bt_evt_cs_read_remote_supported_capabilities_complete_t#

typedef struct sl_bt_evt_cs_read_remote_supported_capabilities_complete_s sl_bt_evt_cs_read_remote_supported_capabilities_complete_t

Definition at line 12357 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_cs_read_remote_supported_capabilities_complete_id#

#define sl_bt_evt_cs_read_remote_supported_capabilities_complete_id
Value:
0x045900a0

Identifier of the read_remote_supported_capabilities_complete event.


Definition at line 12141 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h