sl_bt_evt_sm_passkey_request#
Indicates a request for the passkey prompt displayed on the remote device.
Use the command sl_bt_sm_enter_passkey to input the passkey value.
Modules#
sl_bt_evt_sm_passkey_request_s
Typedefs#
typedef struct sl_bt_evt_sm_passkey_request_s
Macros#
#define
sl_bt_evt_sm_passkey_request_id 0x010f00a0
Identifier of the passkey_request event.
Typedef Documentation#
sl_bt_evt_sm_passkey_request_t#
typedef struct sl_bt_evt_sm_passkey_request_s sl_bt_evt_sm_passkey_request_t
Definition at line
9914
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h