sl_bt_evt_sm_bonding_failed#
This event is triggered if the pairing or bonding procedure fails.
Modules#
sl_bt_evt_sm_bonding_failed_s
Macros#
#define
Identifier of the bonding_failed event.
Typedef Documentation#
sl_bt_evt_sm_bonding_failed_t#
typedef struct sl_bt_evt_sm_bonding_failed_s sl_bt_evt_sm_bonding_failed_t
Definition at line 10008
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_sm_bonding_failed_id#
#define sl_bt_evt_sm_bonding_failed_id
Value:0x040f00a0
Identifier of the bonding_failed event.
Definition at line 9996
of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h