Data structure of the bonding_failed event.

Public Attributes#

uint8_t
uint16_t

Public Attribute Documentation#

connection#

uint8_t sl_bt_evt_sm_bonding_failed_s::connection

Connection handle


Definition at line 10003 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h

reason#

uint16_t sl_bt_evt_sm_bonding_failed_s::reason

An sl_status_t code describing the error that occurred


Definition at line 10004 of file /mnt/raid/workspaces/ws.iS2YF8Lrv/overlay/gsdk/protocol/bluetooth/build/native/sw/bgapi/inc/sl_bt_api.h