Data structure of the report event.
Public Attribute Documentation#
analyzer#
uint8_t sl_bt_evt_connection_analyzer_report_s::analyzer
The handle of the connection analyzer
Definition at line
15408
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
central_rssi#
int8_t sl_bt_evt_connection_analyzer_report_s::central_rssi
RSSI measurement of the packet transmitted by the Central device. Units: dBm.
Range: -127 to +20
Definition at line
15409
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
peripheral_rssi#
int8_t sl_bt_evt_connection_analyzer_report_s::peripheral_rssi
RSSI measurement of the packet transmitted by the Peripheral device. Units: dBm.
Range: -127 to +20
Definition at line
15412
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h