Data structure of the result_continue event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_cs_result_continue_s::connection
Connection handle. Returns a SL_BT_INVALID_CONNECTION_HANDLE (0xFF) when triggered as a result of sl_bt_cs_test_start command
config_id#
uint8_t sl_bt_evt_cs_result_continue_s::config_id
CS configuration identifier. This paremeter is ignored when the event is triggered as a result of sl_bt_cs_test_start command.
Range: 0 to 3
procedure_done_status#
uint8_t sl_bt_evt_cs_result_continue_s::procedure_done_status
Enum sl_bt_cs_done_status_t. Current status of the CS procedure Values:
sl_bt_cs_done_status_complete (0x0): All results complete for the CS procedure or subevent
sl_bt_cs_done_status_partial_results_continue (0x1): Partial results with more to follow
sl_bt_cs_done_status_aborted (0xf): Current procedure and all subsequent subevents in the procedure aborted or current subevent aborted.
subevent_done_status#
uint8_t sl_bt_evt_cs_result_continue_s::subevent_done_status
Enum sl_bt_cs_done_status_t. Current status of the CS subevent Values:
sl_bt_cs_done_status_complete (0x0): All results complete for the CS procedure or subevent
sl_bt_cs_done_status_partial_results_continue (0x1): Partial results with more to follow
sl_bt_cs_done_status_aborted (0xf): Current procedure and all subsequent subevents in the procedure aborted or current subevent aborted.
abort_reason#
uint8_t sl_bt_evt_cs_result_continue_s::abort_reason
Indicates the abort reason when the procedure_done_status or subevent_done_status is set to 0xF, otherwise the default value is set to zero.
Bits 0-3 indicate the procedure abort reasons:
0x0 = Report with no abort
0x1 = Abort because of local Host or remote request
0x2 = Abort because filtered channel map has less than 15 channels
0x3 = Abort because the channel map update instant has passed
0xF = Abort because of unspecified reasons
Bits 4-7 indicate the subevent done reasons:
0x0 = Report with no abort
0x1 = Abort because of local Host or remote request
0x2 = Abort because no CS_SYNC (mode-0) received
0x3 = Abort because of scheduling conflicts or limited resources
0xF = Abort because of unspecified reasons
num_antenna_paths#
uint8_t sl_bt_evt_cs_result_continue_s::num_antenna_paths
Number of antenna paths supported by the local controller for the CS tone exchanges. The number of antenna paths used during the phase measurement stage of the CS step.
Range: 1 to 4
Value: 0. Phase measurement does not occur during the CS step, therefore ignored
num_steps#
uint8_t sl_bt_evt_cs_result_continue_s::num_steps
Number of steps in the CS subevent for which results are reported.
Range: 1 to 160
data#
uint8array sl_bt_evt_cs_result_continue_s::data
The result data is structured as follows:
step_mode: 1 octet for each num_steps. Mode type. Range 0 to 3.
step_channel: 1 octet for each num_steps. Channel index. Range 1 to 78.
step_data_length: 1 octet for each num_steps. Length of mode and role specific information being reported. Range 0x00 to 0xFF.
step_data: step_data_length octet for each corresponding steps in num_steps.