sl_bt_evt_cs_test_end_completed#
This event is generated when the local controller stops the ongoing CS test as the result of calling the sl_bt_cs_test_end command.
Modules#
sl_bt_evt_cs_test_end_completed_s
Typedefs#
Macros#
#define
sl_bt_evt_cs_test_end_completed_id 0x005a00a0
Identifier of the end_completed event.
Typedef Documentation#
sl_bt_evt_cs_test_end_completed_t#
typedef struct sl_bt_evt_cs_test_end_completed_s sl_bt_evt_cs_test_end_completed_t
Definition at line
13772
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
Macro Definition Documentation#
sl_bt_evt_cs_test_end_completed_id#
#define sl_bt_evt_cs_test_end_completed_idValue:
0x005a00a0
Identifier of the end_completed event.
Definition at line
13762
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h