sl_bt_evt_dfu_boot_failure#

This event indicates that an error, which prevents the device from booting, has occurred in bootloader.

Modules#

sl_bt_evt_dfu_boot_failure_s

Macros#

#define

Identifier of the boot_failure event.

Typedef Documentation#

sl_bt_evt_dfu_boot_failure_t#

typedef struct sl_bt_evt_dfu_boot_failure_s sl_bt_evt_dfu_boot_failure_t

Definition at line 200 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_dfu_boot_failure_id#

#define sl_bt_evt_dfu_boot_failure_id
Value:
0x010000a0

Identifier of the boot_failure event.


Definition at line 190 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h