sl_bt_evt_gatt_characteristic#

Indicates that a GATT characteristic in the remote GATT database was discovered.

This event is generated after issuing either the sl_bt_gatt_discover_characteristics or sl_bt_gatt_discover_characteristics_by_uuid command.

Modules#

sl_bt_evt_gatt_characteristic_s

Macros#

#define

Identifier of the characteristic event.

Typedef Documentation#

sl_bt_evt_gatt_characteristic_t#

typedef struct sl_bt_evt_gatt_characteristic_s sl_bt_evt_gatt_characteristic_t

Definition at line 7666 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

Macro Definition Documentation#

sl_bt_evt_gatt_characteristic_id#

#define sl_bt_evt_gatt_characteristic_id
Value:
0x020900a0

Identifier of the characteristic event.


Definition at line 7653 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h