Data structure of the user_write_request event.
Public Attribute Documentation#
connection#
uint8_t sl_bt_evt_gatt_server_user_write_request_s::connection
Connection handle
Definition at line
9395
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
characteristic#
uint16_t sl_bt_evt_gatt_server_user_write_request_s::characteristic
GATT characteristic handle. This value is normally received from the gatt_characteristic event.
Definition at line
9396
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
att_opcode#
uint8_t sl_bt_evt_gatt_server_user_write_request_s::att_opcode
Enum sl_bt_gatt_att_opcode_t. Attribute opcode that informs the procedure from which the value was received.
Definition at line
9399
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
offset#
uint16_t sl_bt_evt_gatt_server_user_write_request_s::offset
Value offset
Definition at line
9402
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h
value#
uint8array sl_bt_evt_gatt_server_user_write_request_s::value
Value
Definition at line
9403
of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h