Data structure of the status event.

Public Attributes#

uint32_t

Public Attribute Documentation#

advertising_set#

uint8_t sl_bt_evt_periodic_advertiser_status_s::advertising_set

The advertising set handle that the periodic advertising is from


Definition at line 3262 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

status#

uint32_t sl_bt_evt_periodic_advertiser_status_s::status

The status value.

Bit 0:

  • 0: The transmission was successful.

  • 1: The transmission failed.

Other bits: Unused and reserved for future


Definition at line 3264 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h

event_counter#

uint16_t sl_bt_evt_periodic_advertiser_status_s::event_counter

The event counter of the transmission


Definition at line 3271 of file /mnt/raid/workspaces/ws.cynwT2I6w/overlay/gsdk/protocol/bluetooth/build/native/ble_host/ble_bgapi/inc/sl_bt_api.h